你好,请问8168的视频捕捉输入Vin0和vin1怎么可以配置成三路1080p/60fps输入?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
cheng fan 说:好的,谢谢您,那单个vout端口是不是也可以配成两个8位的1080p30输出端口?
不可以。你可以在DM816x的数据手册里面找到下面的信息:
• Up to two (one 16-bit, 24-bit, 30-bit and one 16-bit) digital video outputs (up to 165 MHz).
– VOUT[0] can output up to 30-bit video and supports RGB, YUV444, Y and C and BT.656 modes.
– VOUT[1] can output up to 16-bit video and supports Y and C and BT.656 modes.
• Two (one 16-bit, 24-bit and one 16-bit) independently configurable external video input capture ports
(up to 165 MHz).
– 16-bit and 24-bit HD digital video input or dual clock independent 8-bit SD inputs on each capture
port.
• VIN[0] can accept single-channel 16-bit, 24-bit (YCbCr and RGB) video or dual-channel 8-bit
(YCbCr) video.
• VIN[1] can accept single-channel 16-bit (YCbCr) video or dual-channel 8-bit (YCbCr) video.