This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
6614的datasheet(SPRS671D),
2.6.1章节,写着“With ARM as the boot master, two boot modes are chosen by the boot mode sequence. If a failure on the primary
boot mode is detected, then the secondary boot mode is attempted.”
table 2-13 ARM Boot Mode Sequence,里面每一组设置都有两种boot mode(分别为1st和2nd),我以0001组合为例,其对应的boot mode是1st=UART,2nd=EMIF16(NOR),在串口没有接线的情况下,等了好久也没见EMIF16(NOR)有进行boot(在组合1101时,这种bootmode是能正常工作的)。
问题:如何理解上面红色的句子?怎样算primary boot mode failure?
谢谢!
由始至终只改变DEVSTAT寄存器的bit10和bit9,
DEVSTAT value = 0x0001DEA0(1101组合) / 0x0001D8A0(0001组合)
当组合1101时,DEVSTAT值=0x0001DEA0,EMIF16(NOR)先启动,其boot mode配置(bit 6-3)是0100(No wait,16bit,CE0),是可以正常启动的。
当组合0001时,DEVSTAT值=0x0001D8A0,UART先启动,其boot mode配置(bit 6-3)也是0100(无论UART还是EMIF16(NOR)也是这个配置),对于UART来说,只有bit3(值0,表示port 0)是有效的。在串口没有接线的情况下(UART启动显然失败),在ARM bootloader转到EMIF16(NOR)启动时,要如何配置EMIF16(NOR)的boot mode配置?但即使要重配EMIF16(NOR)的boot mode configuration fields,最终也是配回0100吧?