你好,
测试DM36X APPRO 368 的产考设计,软件是 3.1 版, USB 插上U盘后没任何反应。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Alex,
参考设计上的USB是usb device,不是usb host。
DM36x的USB控制器本身是支持USB host,可以借U 盘,相关驱动也是有的。DM36x EVM上是可以验证的。
把设置成host ,模式,启动后
Starting kernel ...
[ 1.080000] usb 1-1: device descriptor read/64, error -19
[ 1.310000] usb 1-1: device descriptor read/64, error -19
[ 1.960000] usb 1-1: device not accepting address 4, error -19
[ 2.500000] usb 1-1: device not accepting address 5, error -19
[ 80.230000] IP-Config: Reopening network devices...
INIT: version 2.86 booting
mknod: /dev/spidev0.0: File exists
Creat queue id:0
queue id:0
FileMngThread created