This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm crrently doing ISP tuning with TDA4 platform. Some questions ragerding this as below.
1. Some plugins were lacked in DCC tool (ver2.0), such as GLBCE, NSF4, DPC, LSC, EE. Is the version correct? Or those plugins are still under developing?
2. Code structure about tuning. Could you help indicate where the code related ISP tuning located in? Whether is the interface avalaible for writing/reading registers of ISP?
I assume it's possible to access ISP registers if DCC tool cannot work well.
SDK:
PROCESSOR-SDK-LINUX-DRA8X-TDA4X V06.02.00.07
PROCESSOR-SDK-RTOS-DRA8X-TDA4X V06.02.00.21
Thanks.
Best regards,
Zhishen