我有这么一个程序:
#include <std.h>
#include <log.h>
#include <clk.h>
#include "L1DRAMcfg.h"
#define N 512
short x[256];
short y[256];
Void task();
/*
* ======== main ========
*/
Void main()
{
LOG_printf(&trace, "hello world!");
/* fall into DSP/BIOS idle loop */
return;
}
Void task()
{
int a[N], b[N];
int i, sum;
// Float timeout, milliSecsPerIntr, cycles;
LgUns start, stop, result;
LOG_printf(&trace, "This is the first task!");
sum = 0;
for(i = 0; i < N; i++)
{
a[i] = i;
b[i] = i;
}
for(i = 0; i < 256; i++)
{
x[i] = i;
y[i] = i;
}
start = CLK_gethtime();
for(i = 0; i < N; i++)
sum += a[i] * b[i];
for(i = 0; i < 256; i++)
sum += x[i] * y[i];
stop = CLK_gethtime();
result = stop - start;
LOG_printf(&trace, "The start time is: %d\n", start);
LOG_printf(&trace, "The stop time is: %d\n", stop);
LOG_printf(&trace, "The result is: %d\n", result);
LOG_printf(&trace, "The sum is: %d\n", sum);
}
然后在CCS 5中debug。我发现在cache view中能看到全局变量x和y的缓存情况,但却看不到局部变量a和b的缓存情况。请问是什么原因?