如题,在追踪串口中断接收字符接口UART_getc() 到底层,其调用的是 typedef int32_t (*UART_ReadPollingFxn) (UART_Handle handle, void *buffer, size_t size);函数指针,但是该原型我并没有检索到,这个函数的具体实现,想要看下,是否在函数内部会将从串口接收的0x0D字符自动转换为0x0A,从而导致上层接收到的字符被意外改变? 如果该函数接口内部并没有进行该操作,那么请问,在初始化该UART Console中,哪项参数可能会造成此现象发生!?
uint8_t UARTGetc(void)
{
return (UARTCharGet(gUartBaseAddr));
}
static int8_t UARTCharGet(uint32_t baseAdd)
{
uint32_t lcrRegValue = 0;
int8_t retVal = 0;
{
uint32_t lcrRegValue = 0;
int8_t retVal = 0;
/* Switching to Register Operational Mode of operation. */
lcrRegValue = UARTRegConfigModeEnable(baseAdd, UART_REG_OPERATIONAL_MODE);
lcrRegValue = UARTRegConfigModeEnable(baseAdd, UART_REG_OPERATIONAL_MODE);
/* Waits indefinitely until a byte arrives in the RX FIFO(or RHR). */
while ((uint32_t) UART_LSR_RX_FIFO_E_RX_FIFO_E_VALUE_0 ==
(HW_RD_REG32(baseAdd + UART_LSR) &
UART_LSR_RX_FIFO_E_MASK))
{
/* Do nothing - Busy wait */
}
while ((uint32_t) UART_LSR_RX_FIFO_E_RX_FIFO_E_VALUE_0 ==
(HW_RD_REG32(baseAdd + UART_LSR) &
UART_LSR_RX_FIFO_E_MASK))
{
/* Do nothing - Busy wait */
}
retVal = (int8_t) HW_RD_REG32(baseAdd + UART_RHR);
/* Restoring the value of LCR. */
HW_WR_REG32(baseAdd + UART_LCR, lcrRegValue);
HW_WR_REG32(baseAdd + UART_LCR, lcrRegValue);
return retVal;
}
}
发现在该函数中并没有涉及对接收到的字符的处理,我之所以确定是接收到的字符被改变是通过单步调试,在确定发送端发出字符为0x0D不被发送端改变(这里我使用俩个串口设备互相检测)的前提下,通过我所提到的调用接口UART_getc内部单步调试查看接收到的字符确实变为0x0A.