This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm 8168 無法decode到 12 ch 問題?



dm 8168 無法decode到 12 ch 問題?

第11個ch可以,

但接到12就不行.

                        h.264                                                *
 *                          |                                                  *
 *                        dec (12 ch)                                                  *
 *                          |
                           que
       |
                          merge
       |                                         *     
 *                         swMs                                                *
 *                          |
 *                         dis

  • 首先,你说无法encode,可是图里画的是decode?

    你说的问题,是第12ch无法创建?还是什么别的问题?

    ch 分辨率是多大?有无出错的log?

  • 抱歉,

    是dec,

    我已設定chains_ipcBits.c 與chains_encDecLoopBack.c

    #define DEC_CH 12
    #define ENC_CH 4
    #define NUM_INST 1

    ch 分辨率 848x480


    在chains_ipcBits.c內將

    #define CHAINS_IPC_BITS_MAX_NUM_CHANNELS                                    (12)

    就會出現錯誤

     

     1506: CHAINS  : CPU Revision [ES1.1] !!!

     1506: CHAINS  : Detected [(null)] Board !!!

     1506: CHAINS  : Base Board Revision [DVR] !!!

     1506: CHAINS  : Daughter Card Revision [DVR] !!!

     

     [host] CHAINS:Enable file write :(y -- yes/n -- no):

     [host]

    CHAINS:Using default file store path:/ti816x


     [host]

    CHAINS:Selected File store path:/ti816x

     [host] CHAINS:Enable file read :(y -- yes/n -- no):

     [host] CHAINS_IPCBITS_SEND:Chains_ipcBitsSendFxn:Entered...

     [host] CHAINS_IPCBITS_RECV:Chains_ipcBitsRecvFxn:Entered...Display 0: Layout: CHAINS_LAYOUT_12ch


     [host]  1852: IPC_BITS_OUT   : Create in progress !!!
    ###Bit buff of size from the SR # 1 : 19906560


     [host] IPC_BITSOUT:BitBuffer Alloc.PoolID:0,Size:0x12FC000

     [host] IPCBITSOUTLINK:Translated Addr Virt:0x2bec8080 To Phy:0x88000080

     [host]  1853: IPC_BITS_OUT   : Create Done !!!
     [m3video]  14717: IPC_BITS_IN   : Create in progress !!!
     [m3video]  14717: SYSTEM: Opening ListMP [HOST_IPC_OUT_24] ...
     [m3video]  14717: SYSTEM: Opening ListMP [HOST_IPC_IN_24] ...
     [m3video]  14718: SYSTEM: Opening MsgQ [HOST_MSGQ] ...
     [m3video]  14720: IPC_BITS_IN   : Create Done !!!
     [m3video]  14720: DECODE: Create in progress ... !!!
     [m3video] DECLINK_H264:HEAPID:0USED:4264
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  14767: DECODE: Creating CH0 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  14813: DECODE: Creating CH1 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  14859: DECODE: Creating CH2 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  14905: DECODE: Creating CH3 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  14951: DECODE: Creating CH4 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  14997: DECODE: Creating CH5 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  15043: DECODE: Creating CH6 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  15089: DECODE: Creating CH7 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  15135: DECODE: Creating CH8 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  15181: DECODE: Creating CH9 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  15227: DECODE: Creating CH10 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video] DECLINK_H264:HEAPID:0USED:2368
     [m3video] DECLINK_H264:HEAPID:3USED:4444160
     [m3video]  15273: DECODE: Creating CH11 of 720 x 480 [PROGRESSIVE] [NON-TILED  ],target bitrate = 2000 Kbps ...
     [m3video]  15274: DECODE: All CH Create ... DONE !!!
     [m3vpss ]  15278: IPC_IN_M3   : Create in progress !!!
     [m3vpss ]  15278: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_0] ...
     [m3video] DECLINK:HEAPID:0USED:30432
     [m3vpss ]  15278: SYSTEM: Opening ListMP [VIDEO-M3_IPC_IN_0] ...
     [m3video] DECLINK:HEAPID:3USED:118358016
     [m3vpss ]  15279: SYSTEM: Opening MsgQ [VIDEO-M3_MSGQ] ...
     [m3video]  15276: DECODE: Create ... DONE !!!
     [m3vpss ]  15280: IPC_IN_M3   : Create Done !!!
     [m3video]  15277: IPC_OUT_M3   : Create in progress !!!
     [m3vpss ]  15284: DUP   : Create Done !!!
     [m3video]  15277: IPC_OUT_M3   : Create Done !!!
     [m3vpss ]  15285: MERGE   : Create Done !!!
     [m3vpss ]  15285: SWMS: Create in progress !!!
     [m3vpss ]  UTILS: DMA: Allocated CH (TCC) = 58 (58)
     [m3vpss ] SWMS: instance 0, sc id 1, start win 0 end win 17
     [m3vpss ]  15460: SWMS    : VipScReq is FALSE!!!
     [m3vpss ]  15605: SWMS0    : Loading Vertical Co-effs (UPSCALE)x ...
     [m3vpss ]  15605: SWMS0    : Loading Horizontal Co-effs (UPSCALE)x ...
     [m3vpss ]  15605: SWMS    : Co-effs Loading ... DONE !!!
     [m3vpss ]  15606: SWMS    : VipScReq is FALSE!!!
     [m3vpss ] AVSYNC:WARNING!! Application wrongly configureddisplayID[-1]. Reseting to correct displayID[0]
     [m3vpss ]  15609: SWMS    : ******* Configuring clock 15 secs...
     [m3vpss ]  15609: SWMS0    : Loading Vertical Co-effs (12/16)x ...
     [m3vpss ]  15609: SWMS0    : Loading Horizontal Co-effs (11/16)x ...
     [m3vpss ]  15610: SWMS    : Co-effs Loading ... DONE !!!
     [m3vpss ]  15610: SWMS0    : Loading Vertical Co-effs (12/16)x ...
     [m3vpss ]  15610: SWMS0    : Loading Horizontal Co-effs (11/16)x ...
     [m3vpss ]  15610: SWMS    : Co-effs Loading ... DONE !!!
     [m3vpss ] 
     [m3vpss ]  *** [SWMS0] Mosaic Parameters ***
     [m3vpss ] 
     [m3vpss ]  Output FPS: 60
     [m3vpss ] 
     [m3vpss ]  Win | Ch  | Input      | Input          | Input         | Input       | Output     |  Output         | Output        | Output      | Low Cost | SWMS | Data  | Blank |
     [m3vpss ]  Num | Num | Start X, Y | Width x Height | Pitch Y / C   | Memory Type | Start X, Y |  Width x Height | Pitch Y / C   | Memory Type | ON / OFF | Inst | Format| Frame |
     [m3vpss ]  ----------------------------------------------------------------------------------------------------------------------------------------------------------------------
     [m3vpss ]    0 |   0 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |    0,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    1 |   1 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |  480,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    2 |   2 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |  960,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    3 |   3 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   | 1440,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    4 |   4 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |    0,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    5 |   5 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |  480,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    6 |   6 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |  960,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    7 |   7 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   | 1440,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    8 |   8 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |    0,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    9 |   9 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |  480,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]   10 |  10 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   |  960,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]   11 |  11 |    0,    0 |   720 x    480 |   896 /   896 | NON-TILED   | 1440,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ] 
     [m3vpss ] SWMS:HEAPID:0USED:424
     [m3vpss ] SWMS:HEAPID:1USED:31392
     [m3vpss ] SWMS:HEAPID:4USED:67921920
     [m3vpss ]  15615: SWMS: Create Done !!!
     [m3vpss ]  15615: DISPLAY: Create in progress !!!
     [m3vpss ]  15616: DISPLAY: Create Done !!!
     [m3vpss ]  15617: DISPLAY: Start in progress !!!


     ====================

     Chains Run-time Menu

     ====================

     

     0: Stop Chain

     

     a: CHAINS_LAYOUT_2x2_

     

     b: CHAINS_LAYOUT_2x2_PLUS_1CH

     

     c: CHAINS_LAYOUT_1x1_PLUS_2CH

     

     s: Switch Display Layout  (Sequential change of layout)

     c: Switch Display Channel (Sequential: Increments by 1)

     p: Print Capture Statistics

     b: Modify Encoder Bit Rate

     f: Modify Encoder Frame Rate

     r: Modify Intra Frame Interval(GOP)

     t: Toggle force IDR frame

     g: Print Encoder Dynamic Parameters

     i: Print IVA-HD Statistics

     m: Print SwMs Statistics

     a: Audio Capture / Playback

     

     Enter Choice:  [m3vpss ]  15651: DISPLAY: Start Done !!!
     [m3vpss ]  15651: DISPLAY: HDDAC(BP0) : 58 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!!


     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0
     [m3vpss ]  15651: SWMS: Start in Progress !!!
     [m3vpss ]  15651: SWMS: Start Done !!!
     [m3vpss ]  15651: DISPLAY: UNDERFLOW COUNT: HDMI(BP0) 1, HDDAC(BP0) 1, DVO2(BP1) 1, SDDAC(SEC1) 1
     [m3vpss ]  15651: SYSTEM  : FREE SPACE : System Heap      = 6192 B, Mbx = 10239 msgs)
     [m3vpss ]  15652: SYSTEM  : FREE SPACE : SR0 Heap         = 11003648 B (10 MB)
     [m3vpss ]  15652: SYSTEM  : FREE SPACE : Frame Buffer     = 188732288 B (179 MB)
     [m3vpss ]  15652: SYSTEM  : FREE SPACE : Bitstream Buffer = 332939136 B (317 MB)
     [m3vpss ]  15652: SYSTEM  : FREE SPACE : Tiler 8-bit      = 89128960 B (85 MB)  - TILER ON
     [m3vpss ]  15652: SYSTEM  : FREE SPACE : Tiler 16-bit     = 44040192 B (42 MB)  - TILER ON


     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0


     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0


     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0


     [host] CHAINS_IPCBITS_SEND:Chains_ipcBitsSendFxn:INFO: periodic print..

     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0
     [c6xdsp ]  19480: Assertion @ Line: 19 in links_common/system/system_linkApi_local.c: linkId < SYSTEM_LINK_ID_MAX : failed !!!
     [m3vpss ]  19568: SYSTEM: Opening MsgQ [DSP_MSGQ] ...
     [m3vpss ]  SWMS: *** UPDATING RT Params ***
     [m3vpss ]  19581: SWMS    : ******* Configuring clock 15 secs...
     [m3vpss ]  19581: SWMS0    : Loading Vertical Co-effs (UPSCALE)x ...
     [m3vpss ]  19581: SWMS0    : Loading Horizontal Co-effs (UPSCALE)x ...
     [m3vpss ]  19581: SWMS    : Co-effs Loading ... DONE !!!
     [m3vpss ]  19581: SWMS0    : Loading Vertical Co-effs (UPSCALE)x ...
     [m3vpss ]  19582: SWMS0    : Loading Horizontal Co-effs (UPSCALE)x ...
     [m3vpss ]  19582: SWMS    : Co-effs Loading ... DONE !!!
     [m3vpss ] 
     [m3vpss ]  *** [SWMS0] Mosaic Parameters ***
     [m3vpss ] 
     [m3vpss ]  Output FPS: 60
     [m3vpss ] 
     [m3vpss ]  Win | Ch  | Input      | Input          | Input         | Input       | Output     |  Output         | Output        | Output      | Low Cost | SWMS | Data  | Blank |
     [m3vpss ]  Num | Num | Start X, Y | Width x Height | Pitch Y / C   | Memory Type | Start X, Y |  Width x Height | Pitch Y / C   | Memory Type | ON / OFF | Inst | Format| Frame |
     [m3vpss ]  ----------------------------------------------------------------------------------------------------------------------------------------------------------------------
     [m3vpss ]    0 |   0 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |    0,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    1 |   1 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |  480,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    2 |   2 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |  960,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    3 |   3 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   | 1440,    0 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    4 |   4 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |    0,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    5 |   5 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |  480,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    6 |   6 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |  960,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    7 |   7 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   | 1440,  360 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    8 |   8 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |    0,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]    9 |   9 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |  480,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]   10 |  10 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   |  960,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ]   11 |  11 |    0,    0 |   512 x    288 |   896 /   896 | NON-TILED   | 1440,  720 |   480 x    360 |  3840 /      0 | NON-TILED   |      ON  |    0 |  420SP |   OFF |
     [m3vpss ] 


     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0


     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0


     [host] $$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$ : 0
     ASSERT (ipcBitsOutLink_tsk.c|IpcBitsOutLink_putFullBufs|955)

  • 你好,我想问一下这个问题你解决没 Assertion @ Line: 19 in links_common/system/system_linkApi_local.c: linkId < SYSTEM_LINK_ID_MAX : failed !!!,我现在也遇到这个问题,望你指教一下

  • dear xing lixing, 

    你可以試著改看看以下設定

    /home/dvr_rdk4.1/RDK4.01/dvr_rdk/mcfw/src_bios6/utils/src/utils_dma_common_cfg.c

    #define UTILS_M3VPSS_EDMACH_ALLOC_1     (0xFE0E0000)//ori: (0xFC000000)

    #define UTILS_C6XDSP_EDMACH_ALLOC_1     (0x01010000) //ori: (0x030F0000)