This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6638硬件平台千兆网口问题



TI工程师你好:

              最近生产了一批板子,发现一个问题c6638的u-boot初始化卡死到sgmii_serdes_setup_156p25mhz函数的

/*Waiting for SGMII Serdes PLL lock.*/
for (cnt = 10000; cnt > 0 && ((readl(0x02090114) & 0x10) == 0);cnt--);卡死,请问这行代码处理的是什么,

参考芯片手册查找00114h Port 1 SGMII STATUS Status Register (read only)

第四位为   4 LOCK Lock. This is the LOCK input pin. Indicates that the SerDes PLL is locked.

请问这块板子的问题出在硬件的什么状态,测量板子硬件有25M时钟。