This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs5.5无法编译DSP6416的DSP/bios例程



正常安装ccs5.5并且建立DSP6416的hello例程,可以正常编译通过,且生成目标码(.out文件),但是尝试打开ccs3.3版本的cdb文件后,再也无法打开例程自带的tcf文件,也无法编译通过,报错如下

在将“ti/bios/config/cdb”文件夹放到安装的根目录下并没有能解决该问题。

重新安装是可以编译通过的,但是我同样没能在安装目录中找到sim64xx的文件夹和c64xx.cdb。

担心以后出现相同的问题,所以来这里请教下。

另外想咨询下,是否可以下载在到类似的bios例程。

  • “但是我同样没能在安装目录中找到sim64xx的文件夹和c64xx.cdb”您的意思重新安装dsp/bios后,还是没能找到sim64xx和c64xx.cdb文件?
  • 是在重新安装ccs5.5后,在"xdctools_3_25_03_72/packages/ti/platform"中并没有找到"sim64xx"的文件夹,但在"……/bios/config/cdb/"中找到了c64xx.cdb。这时候DSP6416的工程可以编译通过。
    所以想咨询下,在ccs5.5(DSP/BIOS5.42.1.09)下打开ccs3.1(BIOS4.90.02.10)的cdb文件是否确定会导致,ccs5.5无法打开DSP6418的TCF文件,并且无法编译通过,错误提示如上图。
    如果不小心导致这种情况,除了重新安装ccs之外,是否还有其他简洁的方法?
  • sim64xx在C:\ti\bios_5_42_01_09\packages\ti\platforms\sim64xx。