OMAP-L138板采用了PHY LAN8710,L138通过MDIO能识别PHY,但网口ping不通。这可能什么原因呢?
uboot版本:u-boot-2010.12-psp03.21.00.04.lcdk;
同样的单板,如果采用C6748,这网口正常工作。
检查u-boot的驱动,发现只有LXT972,DP83848驱动,其他归入一般PHY驱动,这在以前没有发生问题吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OMAPL138使用 : SDK-Linux-omapl138-lcdk-06.03.00.106,和 u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a,
u-boot跑到提示符下,能找到Ethernet PHY,也能读到寄存器的值,但网口不通,这可能是什么原因? PHY是Lan8710;