This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于达芬奇DDR2 PCB Layout&Routing

   我正在设计一款基于DM6467的视频应用,在看DDR2布局布线手册时遇到如下矛盾的说法,请您解答:

 

1,文档DM6467T将DDR2分为两个组,分别等长,但组间不等长

  一、DDR CK&ADDR_CTRL:CK/ADDR_CTRL走线长度要求在CACLM+-50mil,其中CACLM解释为该组(CK和CTRL)最长的曼哈顿距离

二、DQS&DQ:DQ长度要求在DQLM+-50mil,其中DQLM为最长DQ最长的曼哈顿距离

2,通常DDR都与时钟线有等长关系,而且文档SPRAAVOA-July2008 一篇关于TI DDR PCB Routing的文章中说:The maximus trace delay is limited to the longest Manhattan distance of the signals in a clock domain.The rest of the signals in the domain have to be lengthened.即:同一时钟域中信号要与最长的manhadun作为等长target。

综上,DDR的时钟线、地址控制线和DQ、DQS是同一个时钟域,但是分别等长后DQLM和CACLM不等,这就违反了上述同一时钟域要等长的说法。

现在不知道该如何等长,是全部等长呢还是分开等长呢(DQLM比CACLM短500mil)

  • 不需要全部等长,DDR2布线时数据线要等长,地址线等长,控制线等长,是分开等长,不必全部等长。