我用的DVRRDK2.80,DM8168 ,我在系统开机的时候自动加载init.sh load.sh以及应用程序,启动的时候,有时会出现
JFFS2 notice: (911) read_dnode: wrong data CRC in data node at 0x00a9dc28: read 0xc3c93b, calculated 0xb29b1ecc.
接下来本来应该调用init.sh load.sh,貌似都不正常,不知道是不是和jffs2,文件系统有关,断电无法恢复,重刷jffs2正常
DMA: Module install successful, device major num = 251
DRV: Module install successful
DRV: Module built on Jan 22 2013 17:53:19
VPSS_FVID2: create handle is NULL
VPSS_SYSTEM: failed to create handle
VPSS_CORE : failed to init system
vpss: probe of vpss failed with error -22
VPSS_CORE : failed to register ti81xx-vpss driver
ti81xxfb: Unknown symbol vps_grpx_get_ctrl (err 0)
ti81xxfb: Unknown symbol vps_grpx_get_num_grpx (err 0)
ti81xxhdmi: Unknown symbol TI81xx_un_register_display_panel (err 0)
ti81xxhdmi: Unknown symbol TI81xx_register_display_panel (err 0)
JFFS2 notice: (696) check_node_data: wrong data CRC in data node at 0x0c27ecc8: read 0xb2808aef, calculated 0xa31fc222.
正常的打印

错误的打印

best regards
xavier