This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467T开发存储器和音频问题请教



您好!我们现在在开发DM6467T遇到以下两个问题,有近3个月时间一直未解决:
1)内存频率问题
 我们主板原来用的是2片MT47H64M16的128M的内存,总共是256M内存,能够运行在800M频率下,后来改用了,2片MT47H128M16的256M内存,总共是512M内存,在800M频率下数据读写不正常,降频到600M可以正常读写,数据手册上该2种型号芯片除Row线多一根外其他时序也完全一致。请问是否可以是512M内存下,800M频率下运行?如可以,有无建议的方案。
2)声音问题
  我们现在是用了两块AIC32芯片来采集4路单声道音频, DM6467T的mcasp作为slave模式下,可以得到4路音频的数据,其中第一个AIC32的左声道和第二个AIC32的左声道数据能够采集到声音数据,二2片芯片的右声道得到的数据不正确,并且声道数据之间有串扰;
 DM6467T的mcasp作为master模式下,不管如何设置mcasp寄存器,包括ACLKX和AHCLKX等,(AIC32也已经设置为CLKDIV_IN use BCLK模式,BCLK已设置为输入),但无法得到音频数据;
  • 你好,

    1. 请问更换DDR后DDR时序是否根据新的DDR做过调整?

    2. slave模式下,如果配置为只采集一个aic23的左右声道,是否能正确采集?

    master模式下,是否测量mcasp输出了正确的bclk和frame sync?