个位版主你们好:
本人刚接触dvr_rdk,版本是3.00,看了一下mcfw框架上decoder的api "ti_vdec.h",发现里面decoder的buffer只有输入的接口,木有输出的接口,我想对解码后的yuv文件进行分析和处理,不知道是不是要下到link层去把buffer取出来呢?
本人新手,如有错误请版主和各位前辈们指出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
个位版主你们好:
本人刚接触dvr_rdk,版本是3.00,看了一下mcfw框架上decoder的api "ti_vdec.h",发现里面decoder的buffer只有输入的接口,木有输出的接口,我想对解码后的yuv文件进行分析和处理,不知道是不是要下到link层去把buffer取出来呢?
本人新手,如有错误请版主和各位前辈们指出。
dear Haijun Guo
你好,感谢你的回答,我看了一下link层的代码,发现在创建应用时,有一个system_linkcontrol的函数是把你们demo里的ivamap通过ipcmsgq传到各个poccessor里头的,我不是很明白ivamap的意义,也找不着相应解释的文档,希望你们能解释一下~~谢谢
ivamap是 IVAHD MAP,而IVAHD=HDVICP2.0,所以意思就是多通道、多IVAHD下,通道到IVAHD之间的映射关系,用来指示每个IVAHD处理哪几个通道。
当然,如果是用8147、8107,只有一个IVAHD,所有通道都只能在这一个IVAHD上处理,就没有map的意义了。
主要是针对DM8168、8165来说的。
噢~我明白了~~谢谢~~我用的就是dm8168~~不过我明白了~~非常感谢~~