This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教:无法通过仿真器连接DSP芯片



我用DSP2806芯片做的板子,上电后发现,DSP的仿真器无法连接芯片

仿真器型号是ICETEK-5100USB V2.0A 
错误提示:
Error connecting to the target:
Error 0x80000200/-1031
Fatal Error during: OCS,
Device driver: Problem with the Emulation Controller.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.

Sequence ID: 0
Error Code: -1031
Error Class: 0x80000200
I/O Port = 0
Board Name: F28xx XDS510 Emulator
Cpu Name: CPU_1
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.