This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 SRIO: 关于QMSS,CPPI和SRIO Socket



最近想要实现SRIO的驱动,参考PDK的例程时看到关于SRIO_Socket的配置,最终的包应该也是用SRIO_Socket发送出去的,请问:

1. SRIO_Socket是一个什么样的概念?在论坛或是百度搜索没有看到相关的解释

2. 从手册看,除了type9 stream和type11 message需要用到QMSS和CPPI,其他type的发送应该是用不到的,通过直接配置LSU就可以实现发送,那么一样通过SRIO_Socket发送,

(1)SRIO_Socket用到了QMSS和CPPI对吗

(2)是因为它对数据的打包比较方便吗

3. 例程有通过CSL和API实现的,SRIO手册是直接对寄存器进行配置的,看了半天有点糊涂,想要实现基础的NWRITE NREAD DOORBELL,如果是从SRIO_Socket这条路走,请问有什么建议吗

还请不吝赐教,谢谢!

  • socket是SRIO LLD里的概念,跟网络的套接字类似。
    The SRIO driver was designed such that the library could handle all communication protocols. The design was based on the well known BSD socket API which achieves the same by supporting the networking socket API over different protocol families i.e. IPv4, IPv6, IPX etc. From an application perspective; a SRIO socket is basically an endpoint which can be used to send and receive data. The SRIO socket abstracts the inner details of the SRIO peripheral from
    the end user.

    请参考下面的文档。
    read.pudn.com/.../SRIO_SDS11.PDF

    另外,具体的函数定义可以参考pdk_c665x_2_0_13\packages\ti\drv\srio\docs\doxygen\html\index,搜索socket关键字。
  • 谢谢!文档很有启发作用,但是几个问题:

    1. 对于SRIO的端口(port)设置是怎么实现的呢?比如只想用一对RXTX是怎么设置呢?

    下面是例程中device_srio_loopback.c的代码

    /* Enable TLM Base Routing Information for Maintainance Requests & ensure that
    * the BRR's can be used by all the ports. */
    CSL_SRIO_SetTLMPortBaseRoutingInfo(hSrio, 0, 1, 1, 1, 0);
    CSL_SRIO_SetTLMPortBaseRoutingInfo(hSrio, 0, 2, 1, 1, 0);
    CSL_SRIO_SetTLMPortBaseRoutingInfo(hSrio, 0, 3, 1, 1, 0);
    CSL_SRIO_SetTLMPortBaseRoutingInfo(hSrio, 1, 0, 1, 1, 0);

    /* Configure the Base Routing Register to ensure that all packets matching the
    * Device Identifier & the Secondary Device Id are admitted. */
    CSL_SRIO_SetTLMPortBaseRoutingPatternMatch(hSrio, 0, 1, DEVICE_ID2_16BIT, 0xFFFF);
    CSL_SRIO_SetTLMPortBaseRoutingPatternMatch(hSrio, 0, 2, DEVICE_ID3_16BIT, 0xFFFF);
    CSL_SRIO_SetTLMPortBaseRoutingPatternMatch(hSrio, 0, 3, DEVICE_ID4_16BIT, 0xFFFF);
    CSL_SRIO_SetTLMPortBaseRoutingPatternMatch(hSrio, 1, 0, DEVICE_ID2_8BIT, 0xFF);

    以上代码和port的配置是什么关系呢?

    2. 手册的KeyStone Architecture Serial Rapid IO (SRIO)对于RapidIO Feature Support in SRIO中的描述中有Defined as Big Endian这一条,是否在DSP在接收的时候,比如自环,或者从fpga等设备接收还需要进行大小端的转换?

  • 1. 主要是用来配置片内的inbound 的route路由的。可以参考一下附件SRIO编程手册。7266.SRIO_Programming_Performance.pdf

    2. SRIO数据是big endian的。如果DSP工作在little endian模式的话,SRIO接口会把数据自动转换成big endian。FPGA那边如果是小端模式的话,需要转换成大端。