你好!因為我買了C5515的開發板在開發,但發現當開發板上的USB接到Windows 7 (x64)時
Windows的USB裝置會顯示無法辨識該USB,不知能否幫忙告知我該如何處理該問題
因為我需要用USB來傳輸資料,感謝你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CCS v4支持64bit win 7, 请问你的win 7是64-bit的吗?
安装CCS v4时, 注意安装目录, 见下面wiki网站
http://processors.wiki.ti.com/index.php/Using_CCS_with_Windows_Vista_and_7#CCSv4.2F5
是的我電腦是用x64 win7,我有試過x86 XP也是不行
另外C5515的EVM,
Device USB Port With Integrated 2.0
Fixed-Point Digital Signal Processor High-Speed PHY that Supports:
– 16.67-, 13.33-, 10-, 8.33-ns Instruction Cycle – USB 2.0 Full- and High-Speed Device
和
IEEE-1149.1 (JTAG™)
• 4M x 16-Bit Maximum Addressable External
Boundary-Scan-Compatible
如附件圖片,左邊的是ok,右邊的直接接到PC無法辨識