我的板子 点system reset 在线加载程序 就会报错如下:
C66xx_0: Trouble Reading Memory Block at 0x1082a7a8 on Page 0 of Length 0x8: (Error -1202 @ 0x1082A7A8) Device core is hung. The debugger will attempt to force the device to a ready state to recover debug control. Your application's state will be corrupt. You should have limited access to memory and registers, but you may need to reset the device to debug further. (Emulation package 5.1.232.0)
C66xx_0: Trouble Halting Target CPU: (Error -1202 @ 0x0) Device core is hung. The debugger will attempt to force the device to a ready state to recover debug control. Your application's state will be corrupt. You should have limited access to memory and registers, but you may need to reset the device to debug further. (Emulation package 5.1.232.0)
但是 如果点的是cpu reset 或者不点 直接load 就不会有问题 运行程序也正常!
第一次 遇到这问题 何解?
感觉是器件本身有问题了!