因项目需要,公司打算使用C6678,因我是这方面的新手,想请各位解答一下我的疑问,多谢各位
1. DSP用于视频处理,相机接口为cameralink接口,以前用的DM642,资源到了瓶颈,公司想用C6678,第一个问题是,DSP与相机间的接口如何处理比较好,我看到网上有的方案是用FPGA上挂接2块SDRAM,传输完一帧图像后给DSP中断,然后通过EMIF接口发给DSP的DDR3,或者还有更简单的办法?
2. FPGA与6678的接口,我看到有好几种方式,有用hyperlink的,有用SRIO的,也有用EMIF的,请问现在那种技术比较成熟,带宽大概能达到多少?
3. 应用程序方面,既然6678是多核的DSP,到时编写程序时CCS编译的可执行程序能够自动把任务发给处理核心,还是需要在编程过程中就要分配DSP的计算资源?