This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Beagle Bone Black从串口启动问题



您好各位老师,我之前按照BB Black的开源文件自制了一块板子,在主要模块的供电处插入了很小的电阻,其余都没有改动过。

1. 我按照 https://processors.wiki.ti.com/index.php/AM335X_StarterWare_Booting_And_Flashing#AM335X_Flashing_And_Booting 中 “Booting via UART”步骤先将AM335x_starterware\binary\armv7a\cgt_ccs\am335x\beaglebone\bootloader\Release_UART路径的“boot.bin”文件使用Xmodem通过串口发送到板子上,发送结束后,串口提示“Startware AM335x Boot Loader”, 接下来我再用Xmodem发送\AM335x_starterware\binary\armv7a\cgt_ccs\am335x\beaglebone\demo\Release下的“demo.bin”,但发送完后串口就一直没有任何消息了,板子也没有什么反应。

2. 之前还使用001C-XDS100V3仿真器连接JTAG接口,在CCS9中配置了target configuration,但点击测试后的错误如下:

The value is '-233' (0xffffff17).
The title is 'SC_ERR_PATH_BROKEN'.

The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.

看到网上也有很多一样的问题但都没有通用的原因和解决方法,请问一下各位老师这两个问题应该从哪些方面入手呢?谢谢各位。