6747采用spi1的flash方式加载程序,仿真器调试的时候没有问题,但是把程序下载到flash里面,启动后中断没有,那里的问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
多谢Titan的帮助,我一直没用gel文件,这个文件是必须要用的吗?另外您说的GEL文件中对板子进行初始化的代码是这个吗?
OnTargetConnect( )
{
GEL_TextOut( "\nomap-l137 DSP Startup Sequence\n\n" );
Setup_System_Config( ); // Setup Pin Mux and other system module registers
Setup_PLL(); // Setup PLL0 (300MHZ ARM, 300MHz DSP, 133MHz EMIFs
Setup_Psc_All_On( ); // Setup All Power Domains
Setup_EMIFA(); // Async EMIF
Setup_EMIFB(); // Setup SDRAM
GEL_TextOut( "\nStartup Complete.\n\n" );
}
恩,程序里面这两个函数都有。这个是我程序的一个初始化过程,您看看有什么问题没:
PSC_Init(); // Setup_Psc_All_On( )//电源管理寄存器配置
SYSCFG_Init(); // Setup_System_Config( )//系统配置
PLL_Init(); // Setup_PLL()//锁相环锁定过程
EMB_Init(); // Setup SDRAM
GPIO_Init(); // 部分IO设置
TIMER0_TCR=0x0; // 关定时器
HPI_Init(); // HPI初始化
UART0_Init(115200); // 串口0初始化
UART1_Init(115200); // 串口1初始化
SPI1_Init(); // SPI初始化
Edma3Init(); // EDMA3初始化
TIMER1_Init();
MCASP1_Init();
SetupINTC(); // 中断初始化
asm(" NOP 2 ");
CSR=CSR|0x1; // 开中断
while(0==(CSR&0x1));
while(1)
{
led延时闪烁
}
仿真器调试的时候,没有问题,所有中断都可用;把程序下载到flash后,led会闪烁,但是中断没有反应(我让串口中断输出数据),板子重新连接上后,发现CSR寄存器最后两位是1和0,是全局中断没有使能的意思吧?可是程序里面已经使能了