This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
请帮忙看下问题,BIOS的LOG无输出,工程文件在附件!
你用的BIOS5,但是TCF文件里没有看到开启LOG模块,建立LOG实例。你可以参考一下\bios_5_42_00_07\packages\ti\bios\examples\里面的Hello例子,看看如何设置TCF。
Hi, Titan:
我用的板子是DSK6713,用了C:\CCStudio_v3.3\bios_5_31_02\packages\ti\bios\examples\basic\hello\dsk6713下的工程文件,还是无法输出,在/tools/LOG 的下拉菜单中,能找到trace,但就是无输出,请问具体在哪里需要设置?多谢!
我试了一下,可以啊,看下面的操作:
有一点需要说明,CCS5.3对bios5改变了一些特性,就是如果你看不到 LOG_printf 输出信息,你此时暂停CPU,就会看到 LOG_printf信息了。另外,单步调试,也会暂停CPU,也可以看到 LOG_printf信息。你试试。
我单步运行,还是无法输出,在my_hellocfg.h中有如下语句:extern far LOG_Obj trace; 我也将my_hellocfg.h包含进了工程,
cfg是用来配置bios6的,你用的是bios5还是bios6。
Hi,Titan:
下边是我的BIOS设置:每次我新建BIOS,当保存的时候,它是.cdb格式,这时编译会出错,当我重新打开时,它会变成提示变成tcf格式,然后编译通过
CCS是3.1的,BIOS是4.9的,虽然都很老,但也不至于出这种问题。应该是工程的问题。
下面是CCS5.3,里面集成了BIOS5/6,你换换平台吧。
http://processors.wiki.ti.com/index.php/Download_CCS
项目下周要试产了,换平台已经来不及。。。。只能用printf先凑合看看了