在spru773a中有关中断的描述中,The reset interrupt service fetch packet must be located at address 0 ,但在address 0的位置不应该是二级boot代码吗?在address 0到底是二级boot代码还是其他的东西
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在spru773a中有关中断的描述中,The reset interrupt service fetch packet must be located at address 0 ,但在address 0的位置不应该是二级boot代码吗?在address 0到底是二级boot代码还是其他的东西
Interrupt service table base portion of the IST address. This field is cleared to 0 on reset; therefore, upon startup the IST must reside at address 0. After reset, you can relocate the IST by writing a new value to ISTB. If relocated, the first ISFP(corresponding to RESET) is never executed via interrupt processing, because reset clears the ISTB to 0.