大家好,
我在AM4378上同时用到了RMII和MII接口,但在官网的SDK包里没有看到设备树是如何配置的,只有RGMII的配置,请问我在哪里可以找到这两种配置方法?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Shine,你好
我只配置了一个rmii口,只外接了一颗phy芯片RTL8201F,地址为3。重启后居然扫描到两个phy地址:0和3。设置IP地址后,扫描到的两颗phy都可以ping通,但丢包很严重。这怎么会扫描到两个地址的phy芯片,难道设备树配置还有错误吗?
davinci_mdio_default: davinci_mdio_default {
pinctrl-single,pins = <
/* MDIO */
AM4372_IOPAD(0x94c, PIN_OUTPUT | MUX_MODE0) /* (B17) mdio_clk.mdio_clk */
AM4372_IOPAD(0x948, PIN_INPUT | MUX_MODE0) /* (A17) mdio_data.mdio_data */
>;
};
cpsw_default: cpsw_default {
pinctrl-single,pins = <
/* Slave 1, rmii1 */
AM4372_IOPAD(0x90c, PIN_INPUT | MUX_MODE1) /* (B14) mii1_crs.rmii1_crs_dv */
AM4372_IOPAD(0x910, PIN_INPUT | MUX_MODE1) /* (B13) mii1_rx_er.rmii1_rxer */
AM4372_IOPAD(0x914, PIN_OUTPUT | MUX_MODE1) /* (A13) mii1_tx_en.rmii1_txen */
AM4372_IOPAD(0x928, PIN_OUTPUT | MUX_MODE1) /* (B15) mii1_txd0.rmii1_txd0 */
AM4372_IOPAD(0x924, PIN_OUTPUT | MUX_MODE1) /* (A14) mii1_txd1.rmii1_txd1 */
AM4372_IOPAD(0x940, PIN_INPUT | MUX_MODE1) /* (F17) mii1_rxd0.rmii1_rxd0 */
AM4372_IOPAD(0x93c, PIN_INPUT | MUX_MODE1) /* (B16) mii1_rxd1.rmii1_rxd1 */
AM4372_IOPAD(0x944, PIN_INPUT | MUX_MODE0) /* (A16) rmii1_ref_clk.rmii1_refclk */
>;
};
&mac {
slaves = <1>;
pinctrl-names = "default";
pinctrl-0 = <&cpsw_default>;
//dual_emac;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default";
pinctrl-0 = <&davinci_mdio_default>;
status = "okay";
};
// PHY:RTL8201FI-VC-CG, 192.168.1.100
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <3>;
phy-mode = "rmii";
};