=> tftp 0x80000000 uEnv.txt
**************_cpsw_init**************
link up on port 0, speed 100, full duplex
Using ethernet@4a100000device
TFTP from server 192.168.1.200; our IP address is 192.168.1.201 Filename 'uEnv.txt'.
Load address: 0x80000000
Loading: # 55.7 KiB/s done
Bytes transferred = 285 (11d hex)
=> tftp 0x80000000 MLO
**************_cpsw_init**************
link up on port 0, speed 100, full duplex Using ethernet@4a100000 device
TFTP from server 192.168.1.200; our IP address is 192.168.1.201 Filename 'MLO'.
Load address: 0x80000000
Loading: #
Abort
=> tftp 0x80000000 am335x-boneblack.dtb
**************_cpsw_init************** link up on port 0, speed 100, full duplex
Using ethernet@4a100000 device
TFTP from server 192.168.1.200; our IP address is 192.168.1.201 Filename 'am335x-boneblack.dtb'.
Load address: 0x80000000 Loading: #T T T T
Abort
=> tftp 0x80000000 am335x-boneblack.dtb
**************_cpsw_init************** link up on port 0, speed 100, full duplex
Using ethernet@4a100000 device
TFTP from server 192.168.1.200; our IP address is 192.168.1.201 Filename 'am335x-boneblack.dtb'.
Load address: 0x80000000
Loading: T #T T T #T T T T T #T T T