各位专家好:
现在我手上有两个工程需要集成在一起(IPC, net), net接收数据后,启动计算线程8核通过sharedRegion 共同实现算法的计算。8核加载相同的程序镜像, 通过核号的判断实现不同核处理不同的运算和数据获取地址。
现在问题出现在cfg文件。需要修改cfg文件满足ipc 模块和net 模块。工程基于sys/bios。使用到了task, ipc, sharedRegion. 我修改了几个方案,ipc运行不正常,程序不是跑飞了,就是提示ipc注册事件错误等。
net工程的cfg文件如下:
/********************************************************************************************************************
* Specify all needed RTSC MOudles and ocnfigure them. *
********************************************************************************************************************/
var Memory = xdc.useModule('xdc.runtime.Memory');
var BIOS = xdc.useModule('ti.sysbios.BIOS');
var Task = xdc.useModule('ti.sysbios.knl.Task');
var HeapBuf = xdc.useModule('ti.sysbios.heaps.HeapBuf');
var Log = xdc.useModule('xdc.runtime.Log');
/*
** Allow storing of task names. By default if you name a task with a friendly display name it will not be saved
** to conserve RAM. This must be set to true to allow it. We use friendly names on the Task List display.
*/
//Defaults.common$.namedInstance = true;
Task.common$.namedInstance = true;
var Clock = xdc.useModule ('ti.sysbios.knl.Clock');
/*
** Interface with IPC. Depending on the version of BIOS you are using the
** module name may have changed.
*/
/* Use this for pre BIOS 6.30 */
/* var Sem = xdc.useModule ('ti.sysbios.ipc.Semaphore'); */
/* Use this for BIOS 6.30 plus to get the IPC module */
var Sem = xdc.useModule ('ti.sysbios.knl.Semaphore');
var Hwi = xdc.useModule ('ti.sysbios.hal.Hwi');
var Ecm = xdc.useModule ('ti.sysbios.family.c64p.EventCombiner');
/*
** Configure this to turn on the CPU Load Module for BIOS.
**
*/
/*
var Load = xdc.useModule('ti.sysbios.utils.Load');
Load.common$.diags_USER4 = Diags.ALWAYS_ON;
*/
var Diags = xdc.useModule('xdc.runtime.Diags');
/* Load the CSL package */
var Csl = xdc.useModule('ti.csl.Settings');
/* Load the CPPI package */
var Cppi = xdc.loadPackage('ti.drv.cppi');
/* Load the QMSS package */
var Qmss = xdc.loadPackage('ti.drv.qmss');
/* Load the PA package */
var Pa = xdc.useModule('ti.drv.pa.Settings');
/* Load the Platform/NDK Transport packages */
//var PlatformLib = xdc.loadPackage('ti.platform.evmc6678l');
//var NdkTransport = xdc.loadPackage('ti.transport.ndk');
/*
** Sets up the exception log so you can read it with ROV in CCS
*/
var LoggerBuf = xdc.useModule('xdc.runtime.LoggerBuf');
var Exc = xdc.useModule('ti.sysbios.family.c64p.Exception');
Exc.common$.logger = LoggerBuf.create();
Exc.enablePrint = true; /* prints exception details to the CCS console */
/*
** Give the Load module it's own LoggerBuf to make sure the
** events are not overwritten.
*/
/* var loggerBufParams = new LoggerBuf.Params();
loggerBufParams.exitFlush = true;
loggerBufParams.numEntries = 64;
Load.common$.logger = LoggerBuf.create(loggerBufParams);
*/
/*
** Use this load to configure NDK 2.2 and above using RTSC. In previous versions of
** the NDK RTSC configuration was not supported and you should comment this out.
*/
var Global = xdc.useModule('ti.ndk.config.Global');
/*
** This allows the heart beat (poll function) to be created but does not generate the stack threads
**
** Look in the cdoc (help files) to see what CfgAddEntry items can be configured. We tell it NOT
** to create any stack threads (services) as we configure those ourselves in our Main Task
** thread hpdspuaStart.
*/
Global.enableCodeGeneration = false;
/* Define a variable to set the MAR mode for MSMCSRAM as all cacheable */
var Cache = xdc.useModule('ti.sysbios.family.c66.Cache');
//Cache.MAR224_255 = 0x0000000f;
var Startup = xdc.useModule('xdc.runtime.Startup');
var System = xdc.useModule('xdc.runtime.System');
/*
** Create a Heap.
*/
var HeapMem = xdc.useModule('ti.sysbios.heaps.HeapMem');
var heapMemParams = new HeapMem.Params();
heapMemParams.size = 0x300000;
heapMemParams.sectionName = "systemHeap";
Program.global.heap0 = HeapMem.create(heapMemParams);
/* This is the default memory heap. */
Memory.defaultHeapInstance = Program.global.heap0;
Program.sectMap["sharedL2"] = "DDR3";
Program.sectMap["systemHeap"] = "DDR3";
Program.sectMap[".sysmem"] = "DDR3";
Program.sectMap[".args"] = "DDR3";
Program.sectMap[".cio"] = "DDR3";
Program.sectMap[".far"] = "DDR3";
Program.sectMap[".rodata"] = "DDR3";
Program.sectMap[".neardata"] = "DDR3";
//Program.sectMap[".cppi"] = "DDR3";
Program.sectMap[".cppi"] = "L2SRAM";
Program.sectMap[".init_array"] = "DDR3";
//Program.sectMap[".qmss"] = "DDR3";
Program.sectMap[".qmss"] = "L2SRAM";
Program.sectMap[".cinit"] = "DDR3";
Program.sectMap[".bss"] = "DDR3";
Program.sectMap[".const"] = "DDR3";
Program.sectMap[".text"] = "DDR3";
Program.sectMap[".code"] = "DDR3";
Program.sectMap[".switch"] = "DDR3";
Program.sectMap[".data"] = "DDR3";
Program.sectMap[".fardata"] = "DDR3";
Program.sectMap[".args"] = "DDR3";
Program.sectMap[".cio"] = "DDR3";
Program.sectMap[".vecs"] = "DDR3";
Program.sectMap["platform_lib"] = "DDR3";
Program.sectMap[".far:taskStackSection"] = "L2SRAM";
Program.sectMap[".stack"] = "L2SRAM";
Program.sectMap[".nimu_eth_ll2"] = "L2SRAM";
Program.sectMap[".resmgr_memregion"] = {loadSegment: "L2SRAM", loadAlign:128}; /* QMSS descriptors region */
Program.sectMap[".resmgr_handles"] = {loadSegment: "L2SRAM", loadAlign:16}; /* CPPI/QMSS/PA Handles */
Program.sectMap[".resmgr_pa"] = {loadSegment: "L2SRAM", loadAlign:8}; /* PA Memory */
Program.sectMap[".far:IMAGEDATA"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_OBJMEM"] = {loadSegment: "L2SRAM", loadAlign: 8};
Program.sectMap[".far:NDK_PACKETMEM"] = {loadSegment: "L2SRAM", loadAlign: 128};
/* Required if using System_printf to output on the console */
SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
/*
** Register an EVM Init handler with BIOS. This will initialize the hardware. BIOS calls before it starts.
**
** If yuo are debugging with CCS, then this function will execute as CCS loads it if the option in your
** Target Configuraiton file (.ccxml) has the option set to execute all code before Main. That is the
** default.
*/
//
/*
** Create the stack Thread Task for our application.
*/
var ndkTaskParams = new Task.Params();
ndkTaskParams.stackSize = 8192;
ndkTaskParams.priority = 0x5;
Task.create("&NetStartup", ndkTaskParams);
/*
** Create a Periodic task to handle all NDK polling functions.
** If you are using RTSC configuration with NDK 2.2 and above, this is done by default and
** you do not need to do this.
*/
/*var prdNdkClkParams = new Clock.Params ();
prdNdkClkParams.period = 0x64;
prdNdkClkParams.startFlag = true;
Program.global.clockInst1 = Clock.create("&llTimerTick", 5, prdNdkClkParams);
*/
/*
** If you are using RTSC configuration with NDK 2.2 and above, this is done by default, else
** register hooks so that the stack can track all Task creation
Task.common$.namedInstance = true;
Task.addHookSet ({ registerFxn: '&NDK_hookInit', createFxn: '&NDK_hookCreate', });
*/
/* Enable BIOS Task Scheduler */
BIOS.taskEnabled = true;
/*
* Enable Event Groups here and registering of ISR for specific GEM INTC is done
* using EventCombiner_dispatchPlug() and Hwi_eventMap() APIs
*/
Ecm.eventGroupHwiNum[0] = 7;
Ecm.eventGroupHwiNum[1] = 8;
Ecm.eventGroupHwiNum[2] = 9;
Ecm.eventGroupHwiNum[3] = 10;
//////////////////////////////////////////////////////////////////////////////////////////////
//////////////////////////////////////////////////////////////////////////////////////////////
IPC sharedRegion工程的cfg文件如下 ;
var System = xdc.useModule('xdc.runtime.System');
var SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
/* 存储空间分配 */
Program.sectMap["SystemHeap"] = "L2SRAM";
Program.sectMap[".const"] = "L2SRAM";
Program.sectMap[".switch"] = "L2SRAM";
Program.sectMap[".cinit"] = "L2SRAM";
Program.sectMap[".vecs"] = "L2SRAM";
Program.sectMap[".DDR3_0"] = "DDR3";
var BIOS = xdc.useModule('ti.sysbios.BIOS');
BIOS.heapSize = 0x8000;
/* 创建任务 */
var Task = xdc.useModule('ti.sysbios.knl.Task');
var tsk0 = Task.create('&tsk0_func');
tsk0.instance.name = "tsk0";
/* 创建信号量 */
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
Program.global.semHandle = Semaphore.create(0);
/* 配置核心名 */
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
var procNameAry = MultiProc.getDeviceProcNames();
//var procNameAry = [ "CORE0", "CORE1"];
MultiProc.setConfig(Program.global.procName, procNameAry);
/* IPC 配置 */
var Ipc = xdc.useModule('ti.sdo.ipc.Ipc');
var Notify = xdc.useModule('ti.sdo.ipc.Notify'); /* Notify */
var GateMP = xdc.useModule('ti.sdo.ipc.GateMP'); /* GateMP */
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion'); /* shared region */
var MessageQ = xdc.useModule('ti.sdo.ipc.MessageQ'); /* MessageQ */
var HeapBufMP = xdc.useModule('ti.sdo.ipc.heaps.HeapBufMP');
Ipc.procSync = Ipc.ProcSync_ALL; /* Ipc_start 里同步所有核心*/
Ipc.sr0MemorySetup = true;
GateMP.maxRuntimeEntries = 4;
GateMP.RemoteCustom1Proxy = xdc.useModule('ti.sdo.ipc.gates.GateMPSupportNull');
/* 配置 SharedRegion #0 (IPC) */
var SHAREDMEM = 0x80000000;
var SHAREDMEMSIZE = 0x00100000;
SharedRegion.setEntryMeta(0,
{ base: SHAREDMEM,
len: SHAREDMEMSIZE,
ownerProcId: 0,
isValid: true,
name: "DDR2_RAM",
});
for (var i = 0; i < MultiProc.numProcessors; i++) {
Ipc.setEntryMeta({
remoteProcId: i,
setupMessageQ: true,
});
}
var Startup = xdc.useModule('xdc.runtime.Startup');
还请高手看一下,怎么修改能使用程序正常运行?或给一些修改建议。我是新手,这部分内容以及某些规则还不是很熟悉。
谢谢啦