现在遇到比较怪的问题。我们使用DSP0-C6678 的SRIO Lane1与FPGA-V5连接(1.25G,FPGA为Master,DSP0为Slaver),通信没有问题;使用DSP0的Lane2与另一片DSP1的Lane0连接时采用5G测试也没问题,但是在两个DSP之间采用1.25G和2.5G时会出问题,不能正常通信,提示在返回ACKID的地方有问题,检测一直过不去,程序用的是Keystone_SRIO测试程序。哪位大侠遇到过相同的情况或者指出可能存在问题的地方?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
"返回ACKID有问题",说的太模糊啊。
首先要分清是传输的问题还是建立连接(初始化端口,或者switch连接之类的)的问题,然后再判断是什么问题。
建议最好能看到错误状态,描述下几个关键寄存器的值。