This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DSP280049中运行CLB模块例程的问题



在学习DSP280049C的过程中,学习运行TI的官方例程,但在debug关于CLB模块的程序时即报错(其他程序可以通过),报错内容为:

Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 9.2.0.00002)

请问这种问题应该如何处理呢