This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在官方给的SRIO例程的基础上C6678 SRIO_SERDES_LOOPBACK测试时,数据从DDR读出,然后写入DDR,测试1X、2X、4X模式速率发现2X模式是1X的两倍速,但是4X模式却没有1X模式的四倍,且差的很多,我降低SRIO的速度,2.5Gbps依然是达不到,请问是什么原因?
请试试增加 Payload size。请参考附件SRIO的性能测试数据。1512.Throughput Performance Guide for C66x KeyStone Devices (Rev. A) (2).pdf
您好shine。我测试的通过LL2->LL2在5Gbps,4X模式下接近1x的四倍,但是通过DDR->DDR时速度却有8.6Gbps,请问是不是CPU进行数据搬移速度跟不上,可不可以用EDMA来完成数据从DDR3的搬移呢?然后再通过SRIO传输