This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于EVM中C6678部分IO的串接电阻



最近在看EVM的原理图,想学着做一块板子,遇到了如下几个问题

望TI的FAE们不吝赐教,多谢了~~~

1. EVM中DSP的GPIO与FPGA相连,有10欧姆的电阻串接,想问问为什么需要这个10欧姆,是为了50欧姆的匹配吗?难道DSP的GPIO输出电阻为40欧?从哪查这些数据?这些10欧电阻在布线时需要考虑哪些?靠近DSP的GPIO端?

2. EVM中DSP的GPIO用了4.7K上拉到1.8V,想问问为什么用4.7K?从哪查相关数据?

3. 同时还有EMIF的CE引脚也串接了22欧姆到FPGA,为什么?

4. DSP的RSV引脚除了RSV01、RSV08之外,其他的RSV引脚全都不接,应该没问题吧?EVM中是NC,或者接0欧姆到地,我不想引出,弄一堆空焊盘在板子上。这些RSV引脚直接不引出来,没有问题吧?

5. DSP中的一些端口,例如TSIP、SGM、MDIO等等,我不用。那么这些引脚,直接就不引出来了,没有问题吧?或者应该怎么处理?

请各位不吝赐教~~~真心感谢了!!