您好,
我在正常运行的TDA2X(dra7x)平台上(此时已经有图像输出,运行正常),连接XDS110,可以正常launch,xml文件。但是无法连接到A15或者M4,DSP等任何一个core上,反复上电,执行system reset 也不行。请问应该如何操作才能debug?
警告信息:
ARP32_EVE_1: GEL Output: --->>> Configuring EVE Memory Map <<<---
ARP32_EVE_1: GEL Output: --->>> EVE Memory Map Done! <<<---
ARP32_EVE_2: GEL Output: --->>> Configuring EVE Memory Map <<<---
ARP32_EVE_2: GEL Output: --->>> EVE Memory Map Done! <<<---
ARP32_EVE_3: GEL Output: --->>> Configuring EVE Memory Map <<<---
ARP32_EVE_3: GEL Output: --->>> EVE Memory Map Done! <<<---
ARP32_EVE_4: GEL Output: --->>> Configuring EVE Memory Map <<<---
ARP32_EVE_4: GEL Output: --->>> EVE Memory Map Done! <<<---
CortexA15_0: Failed System Reset: (Error -6306) Failed to connect to PRSC module. (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
CortexA15_0: GEL Output: --->>> IPU1SS Initialization is in progress ... <<<---
TDA2xx_MULTICORE_EnableAllCores() cannot be evaluated.
Could not write 0x4AE06510: target is not connected
at *((unsigned int *) ((cpu_num==1) ? (((0x4AE00000+0x6000)+0x500)+0x10) : (((0x4AE00000+0x6000)+0x700)+0x210)))=(unsigned int) 0x7 [TDA2xx_multicore_reset.gel:12]
at IPUSSClkEnable(1) [TDA2xx_multicore_reset.gel:311]
at IPU1SSClkEnable_API() [TDA2xx_multicore_reset.gel:279]
at TDA2xx_MULTICORE_EnableAllCores()IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.27.9)