用的是官方给的K1 STK V1.1 中的srio例程 测试的是digital loopback 在6678上测试的时候出现了以下问题 数据不匹配。
请问这是什么问题?那一块出问题了 要怎么解决呢?
SWRITE from 0x10802200 to 0x82014000, 8 bytes, 4125 cycles, 15 Mbps, completion code = 0
data mismatch at unit 0, 0x1b (at 0x10802200) != 0x0 (at 0x82014000)
SWRITE from 0x10802200 to 0x82014000, 16 bytes, 4488 cycles, 28 Mbps, completion code = 0
data mismatch at unit 0, 0x1c (at 0x10802200) != 0x0 (at 0x82014000)
SWRITE from 0x10802200 to 0x82014000, 32 bytes, 4494 cycles, 56 Mbps, completion code = 0
data mismatch at unit 0, 0x1d (at 0x10802200) != 0x0 (at 0x82014000)
SWRITE from 0x10802200 to 0x82014000, 64 bytes, 4836 cycles, 105 Mbps, completion code = 0
data mismatch at unit 0, 0x1e (at 0x10802200) != 0x0 (at 0x82014000)
SWRITE from 0x10802200 to 0x82014000, 128 bytes, 5356 cycles, 191 Mbps, completion code = 0
data mismatch at unit 0, 0x1f (at 0x10802200) != 0x0 (at 0x82014000)
SWRITE from 0x10802200 to 0x82014000, 256 bytes, 6242 cycles, 328 Mbps, completion code = 0
data mismatch at unit 0, 0x20 (at 0x10802200) != 0x0 (at 0x82014000)
SWRITE from 0x10802200 to 0x82014000, 512 bytes, 8327 cycles, 491 Mbps, completion code = 0
data mismatch at unit 0, 0x21 (at 0x10802200) != 0x0 (at 0x82014000)
SWRITE from 0x10802200 to 0x82014000, 1024 bytes, 12475 cycles, 656 Mbps, completion code = 0
data mismatch at unit 0, 0x22 (at 0x10802200) != 0x0 (at 0x82014000)