在移植根文件系统到nandflash时,遇到以下报错
UBI error: cannot open mtd NAND.file-system, error -2
[ 1.631751] input: gpio_buttons@0 as /devices/platform/gpio_buttons@0/input/input0
[ 1.640997] hctosys: unable to open rtc device (rtc0)
[ 1.647613] ALSA device list:
[ 1.650692] No soundcards found.
[ 1.655114] VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0): error -19
[ 1.663474] Please append a correct "root=" boot option; here are the available partitions:
[ 1.672148] 0100 65536 ram0
[ 1.672154] (driver?)
[ 1.678359] 0101 65536 ram1
[ 1.678363] (driver?)
[ 1.684591] 0102 65536 ram2
[ 1.684594] (driver?)
[ 1.690778] 0103 65536 ram3
[ 1.690781] (driver?)
[ 1.696999] 0104 65536 ram4
[ 1.697002] (driver?)
[ 1.703213] 0105 65536 ram5
[ 1.703216] (driver?)
[ 1.709412] 0106 65536 ram6
[ 1.709415] (driver?)
[ 1.715627] 0107 65536 ram7
[ 1.715631] (driver?)
[ 1.721761] 0108 65536 ram8
[ 1.721763] (driver?)
[ 1.727914] 0109 65536 ram9
[ 1.727917] (driver?)
[ 1.734065] 010a 65536 ram10
[ 1.734068] (driver?)
[ 1.740282] 010b 65536 ram11
[ 1.740284] (driver?)
[ 1.746544] 010c 65536 ram12
[ 1.746547] (driver?)
[ 1.752780] 010d 65536 ram13
[ 1.752783] (driver?)
[ 1.758997] 010e 65536 ram14
[ 1.759000] (driver?)
[ 1.765232] 010f 65536 ram15
[ 1.765235] (driver?)
[ 1.771457] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 1.779768] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) ]---
网上搜索后找到以下链接的方法:
processors.wiki.ti.com/.../UBIFS_Support
但在使用sd卡启动是发现mtd无显示,信息·如下
root@am335x-evm:/dev# cat /proc/mtd
dev: size erasesize name
请问这是什么情况