This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP C6671和FPGA的SRIO初始化问题



 想请教大家一个SRIO初始化的问题,问题详细描述如下:

     DSP采用TMS320C6671,FPGA采用Xilinx的XC7K325T,配置是1x,DSP的SRIO时钟是250M,速率为2.5G,FPGA的SRIO时钟是125M,速率是2.5G,即DSP和FPGA的速率一样,DSP自环时,通信正常,SP_ERR_STAT的PORT OK有置1,但是DSP和FPGA之间通过SRIO通信时,则出现FPGA初始化不成功,DSP也初始化不成功,必须是FPGA先初始化成功了,DSP初始化时才能与FPGA链接成功吗?数据手册上没有看到有关FPGA和DSP谁先初始化,谁后初始化的问题。

    在FPGA和DSP的SRIO初始化时,FPGA可以看到有数据,但是最后还是初始化失败,是不是由于FPGA高速BANK的相邻时钟对其产生干扰了。