你好,我在使用AWR1642+DCA1000采集数据的时候,出现错误。使用mmWave Studio02_01_01_00,connection选项没有问题,都能正确连接,Static Config、Date Config也没有问题,在Sensor Config里点击Set Up DCA1000时报错
代码显示
[13:37:41] [RadarAPI]: ar1.GetCaptureCardDllVersion()
[13:37:42] [RadarAPI]: Sending dll_version command to DCA1000
[13:37:42] [RadarAPI]:
[13:37:42] DLL Version : 1.0
[13:37:42] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[13:37:42] [RadarAPI]: Status: Passed
[13:37:44] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[13:37:44] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
[13:37:44] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[13:37:44] [RadarAPI]: Sending fpga command to DCA1000
[13:37:55] [RadarAPI]:
[13:37:55] FPGA Configuration :
[13:37:55] Timeout Error! System disconnected
[13:37:55] [RadarAPI]: Sending record command to DCA1000
[13:38:06] [RadarAPI]:
[13:38:06] Configure Record :
[13:38:06] Timeout Error! System disconnected
[13:38:06] [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
[13:38:06] [RadarAPI]: Sending fpga_version command to DCA1000
[13:38:17] [RadarAPI]:
[13:38:17]
[13:38:17] Unable to read FPGA Version. [error -5]
[13:38:17]
一个月前用过这块DCA1000采集数据,没有任何问题,这次使用的时候报错,换了另外一块DCA1000可以正常采集数据。请问这个问题有可能是什么原因导致的?要怎么解决这个问题?