This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ACPY3的2D1D传输



在6467上面用ACPY3做了两组实验,发现2D1D传输的速度巨慢。具体情况是这样的,源和目的内存的地址都是128对齐的。

实验1:

1D1D的传输,内存大小为4M,整个耗时在5-6ms之间。

试验2:

2D1D的传输,内存大小仍然为4M,其他参数如下

elemenSize=1

srcElementIndex=4

numElements=65280

numFrames=0

即源内存大小为4M,目的内存从源内存中4选1,即目的内存的大小为1M

受numElements的限制,本来应该是65535,但是我为了考虑对其的问题,故意设成了65280(256的倍数)。4M的内存分4M/(65280*4)次传送,零头部分不处理。最后总的时间在28-30ms之间。

这种抽样的过程本来就是想通过2D1D的支持来获取高性能,可惜事与愿违。

1D和2D的差异为什么这么大呢?是我有什么地方处理的不对,还是ACPY3的效果就是这样?

有人能告诉我为什么吗?小弟不胜感激呀

  • 具体耗时记不太清楚了,但是有如下结论

    1. EDMA配置Para的时间是很长的

    2. 2D本质就是1D的一个Chain,只不过你只需要启动一次就可以完成

    3. ACPY = Asynchronous Copy

    4. 本质上说,DM3和DM6系列的EDMA就是普通的,DM8的DMA才是非常适合Video类的操作