This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于335x采用dm9000扩展第三个网口的问题



应用场景:

DM9000扩展第三个网口,连接在GPMC接口,和nand共用接口,另外两个网口采用芯片自己的以太网mii连接phy

问题描述

现在三个网口中,DM9000的网口单独接到网络上网络连接正常,但是如果同时把芯片自己的的网口接到网络上,DM9000的网口工作异常,ping包超时或者丢失,而芯片自己的网口工作正常不受影响,拔掉芯片自己的网口的网线,单独使用dm9000,dm9000网卡又恢复正常工作。

1、已经确认三个网口ip设置在不同的网段;

2、已经确认默认网关路由对应正确的网口;

3、采用的是DM9000CP,按照论坛已经将总线的驱动电流调整到8ma,现象依旧;

现在没有思路解决这个问题,希望论坛大神们能帮我找找问题原因,谢谢