This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LVDS324支持MN34041的问题



      你好,

          前面使用的sensor是松下MN34041sensor模式是1080P30Hz。LVDS324的配置为:地址0922,地址0a61,其他为默认。LVDS324寄存器能够正常访问。对324的配置是在对041配置之前完成的。041LVDS时钟和数据直接连到324的相关端口上。

         现在情况是LVDS324的寄存器显示PLL已锁定(地址0a[7]为1'b1),并且地址11寄存器值为0(无识别码错误),其他示波器点出LVDS324确实有74.25MHz的稳定输出,但是无数据和行场信号(数据全部为高,行场全部为低)。

        请问LVDS324到底是否支持MN34041,或者是否有配置上未注意到的地方?