This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教,如何配置6630K2L中DFE模块编程接口函数Dfe_progCfrCoeff的输入参数(numCoeffs、cfrCoeff_i及cfrCoeff_q)?



TI的工程师:

    您好,我们的项目使用的是TCI6630K2L处理器,目前想通过调整DFE中CFR模块的参数来降低发送天线的峰均比(PAR)。我在芯片的SDK安装目录packages\ti\drv\dfe\docs下找到了DFE模块的编程接口文档DFE_LLD_SDS.pdf,依据DFE_LLD_SDS的描述,可以通过接口函数

DFE_Err Dfe_progCfrCoeff
(
DFE_Handle hDfe,
uint32_t cfrDev,
uint32_t numCoeffs,
uint32_t *cfrCoeff_i,
uint32_t *cfrCoeff_q
);

来调整PAR,而且上述接口输入参数numCoeffs的取值范围是0~256,cfrCoeff_i和cfrCoeff_q的取值范围是0~4095,我的问题是

1. numCoeffs的意义是什么?在实际操作中依据什么标准选择该值?

2. 每个Coeff值的意义是什么?在实际操作中依据什么标准选择该值?

  • 感谢您对TI产品的关注!请您将MYTI账号邮箱更改为公司域名邮箱,到英文论坛发帖咨询相关问题。新的电子邮件地址权限最多可能需要15分钟才能生效。您可以在更新邮箱15分钟后重新登陆论坛发帖。
    您也可以浏览此帖了解E2E英文支持论坛的新帖要求: e2e.ti.com/.../94449