This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027的数字比较器事件控制PWMA、PWMB问题



程序说明:使用模拟比较器产生数字比较器事件,强制使PWM1A为低,强制使PWM1B为高。但实测PWM1B波形应该为高电平却为低电平,折腾了好几天,都没解决。请TI工程师和大家帮我看下,是不是配置有不对。

void Init_Comp(void)
{
EALLOW;
GpioCtrlRegs.AIOMUX1.bit.AIO2 = 2;                      // CMP1A,即模拟比较器+输入
Comp1Regs.COMPCTL.bit.COMPDACEN = 1;       //DAC逻辑上电
Comp1Regs.COMPCTL.bit.COMPSOURCE = 0;    // 比较器负极接DAC,即模拟比较器-输入
Comp1Regs.COMPCTL.bit.CMPINV = 0;                // 同相输出,过流输出高
Comp1Regs.COMPCTL.bit.QUALSEL = 0x09;
Comp1Regs.COMPCTL.bit.SYNCSEL = 1;             // 比较器输出在经过ETPWM/GPIO模块前进行同步
Comp1Regs.DACCTL.bit.DACSOURCE = 0;          // DACVAL控制DAC
Comp1Regs.DACVAL.all = 0x0200;                        // 1.65V

EPwm1Regs.DCTRIPSEL.bit.DCAHCOMPSEL = DC_COMP1OUT;   // DCAH输入的源是COMP1OUT
EPwm1Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAH_HI;                       // DCAH为高时DCAEVT2有效(输出高)
EPwm1Regs.DCACTL.bit.EVT2SRCSEL = DC_EVT2;                        // DCAEVT2信号不经过滤波,直通。
EPwm1Regs.DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC;  // 异步,无需同步。
EPwm1Regs.TZSEL.bit.DCAEVT2 = 1;                                                // 允许DCAEVT2作为ePWM1A的周期触发源。
EPwm1Regs.TZCTL.bit.DCAEVT2 = TZ_FORCE_LO;                        // 强制EPWM1A处于低电平

EPwm1Regs.DCTRIPSEL.bit.DCBHCOMPSEL = DC_COMP1OUT;  // DCBH输入的源是COMP1OUT,过流时COMP1OUT为高,
EPwm1Regs.TZDCSEL.bit.DCBEVT2 = TZ_DCBH_HI;                      // DCBH为高时DCAEVT2有效(输出高)
EPwm1Regs.DCBCTL.bit.EVT2SRCSEL = DC_EVT2;                       // DCBEVT2信号不经过滤波,直通。
EPwm1Regs.DCBCTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC;  // 异步,无需同步。
EPwm1Regs.TZSEL.bit.DCBEVT2 = 1;                                               // 允许DCBEVT2作为ePWM1B的周期触发源。
EPwm1Regs.TZCTL.bit.DCBEVT2 = TZ_FORCE_HI;                        // 强制EPWM1B处于高电平
EDIS;
}

下图是没有使用数字比较器时的波形如下,PWM1A和PWM1B互补,是对的。

如程序那样,使用了模拟比较器产生数字比较器事件后,波形始下: