This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x 的Wait0与MII2_CRS信号冲突问题

Other Parts Discussed in Thread: AM3352

由于想使用双网口,并且其中一个PHY要经过连接器,为了降低信号速率,降低连接器成本,需要使用25MHz的MII接口。

分配资源时发现MII2_CRS与GPMC_Wait0是一个引脚,这样就会影响AM3352从NAND Flash启动的设计,那么请问:

1:如何处理这种情况?

2:实际上,以太网已固定工作在全双工模式,那么MII2_CRS是否还必须要用外部信号处理?

使用的AM3352为ZCZ封装。

谢谢。