This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 【分享】Sitara系列产品usb模块简介




  • Sitara usb模块概述

1.两个支持DRD功能的usb模块,也就是usb模块可以根据连接的usb线工作在host或者device两种模式

DRD= Dual-role* Device

2.支持host-only,device-only,DRD模式

3.集成phy,不需要外部的usb phy

4. 每个usb模块具有31个端点,包括15个TX,15个RX和一个双向端点0

  • 特征对比

Note:

*AM57x的第二个usb模块(usb2)不支持SuperSpeed USB

  • ROM usb boot

Note:

*memory boot模式下不支持usb hub

**usb1是am57x的第一个usb模块

  • AM335x EVM板中的usb设计

  • AM437x EVM板中的usb设计

  • AM57x EVM板中的usb设计

Note:

*GP EVM板上的usb1模块有一个SS USB HUB