This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] 【分享】如何使用AM335x 的ehrpwm1/PCB文件打开后空白



如何使用AM335x 的ehrpwm1?

Q: 把EHRPWM1A用作了背光,如何控制EHRPWM1B的输出?

A:配置步骤如下:
1.在设备树中配置ehrpwm管脚复用模式和新建节点。
ehrpwm1_pins: pinmux-ehrpwm1-pins {
pinctrl-single,pins = <
AM33XX_IOPAD(0x848, PIN_OUTPUT_PULLDOWN | MUX_MODE6) /* gpmc_a2.ehrpwm1a */
AM33XX_IOPAD(0x84c, PIN_OUTPUT_PULLDOWN | MUX_MODE6) /* gpmc_a2.ehrpwm1b */
>;
};

&epwmss1 {
status = "okay";

ehrpwm1: pwm@48302200 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&ehrpwm1_pins>;
};
};

2.需要使用 echo 1 > export ,pwmchip0才会显示pwm1.

3. ehrpwm1a和ehrpwm1b必须使用相同的频率。

PCB文件打开后空白

Q: AM571x EVM CAD Files— SPRR241.ZIP中PCB 文件打开后空白,不管是用allegro 16.6或者17.4。

A: 此类问题一般是TI的文件和PCB软件工具的版本和兼容性问题引起的。上述问题把文件名改短后就可以打开了。