This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x连接一个外接的HIDKeyBoard无法输入

Other Parts Discussed in Thread: CC2564MODN

Ti am335x版子上连接了一个标准的输入设备HIDKeyBoard,USB连接,并且设备成功连接打开了,用函数gets(),但是没有输入返回,请问这是怎么回事?

  • 请问是开发板吗?是哪款开发板?使用的哪个SDK版本?请详细说明。
  • SDK是6.0的,不是开发板,是我们这边自己弄的版子,集成了am335x的芯片
  • 我需要咨询一下相关工程师再给您回复,请问是跑的linux吗?相关的启动log是否可以贴出来看一下。
  • 是跑的Linux,
    [ 1.624450] usb 1-1: new full-speed USB device number 2 using musb-hdrc
    [ 1.793640] usb 1-1: New USB device found, idVendor=26f1, idProduct=8801
    [ 1.800659] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
    [ 1.808288] usb 1-1: Product: HIDKeyBoard
    [ 1.812530] usb 1-1: Manufacturer: TMS
    [ 1.816436] usb 1-1: SerialNumber: 1234567890abcd
  • 请参考以下帖子的回复,并提供完整的log。
    e2e.ti.com/.../3633295
  • 那个帖子我好像回不了,我把log贴在这里,麻烦你帮我转过去,谢谢
    U-Boot SPL 2013.01.01-g07d175f-dirty (Sep 14 2015 - 17:16:53)
    only for Mediate WIFI Probe!
    mpu_pll = 550 MHz


    U-Boot 2013.01.01-g07d175f-dirty (Sep 14 2015 - 17:16:53)

    DRAM: 64 MiB
    WARNING: Caches not enabled
    NAND: WP
    512 MiB
    MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
    Using default environment

    In: serial
    Out: serial
    Err: serial
    Net: Net Initialization Skipped
    No ethernet found.
    Hit any key to stop autoboot: 0
    Booting from nand ...

    NAND read: device 0 offset 0x280000, size 0x2b8888
    2853000 bytes read: OK
    ## Booting kernel from Legacy Image at 80007fc0 ...
    Image Name: Linux-3.2.0-ga75e3d3
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 2724224 Bytes = 2.6 MiB
    Load Address: 80008000
    Entry Point: 80008000
    XIP Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux... done, booting the kernel.
    [ 0.000000] Linux version 3.2.0-ga75e3d3 (keanu@KeanusUbuntu) (gcc version 4.7.3 20130226 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.03-20130313 - Linaro GCC 2013.03) ) #262 Wed Aug 24 16:40:06 CST 2016
    [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7d
    [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [ 0.000000] Machine: am335xevm
    [ 0.000000] Memory policy: ECC disabled, Data cache writeback
    [ 0.000000] AM335X ES2.1 (neon )
    [ 0.000000] Built 1 zonelists in Zone order, mobility grouping off. Total pages: 16256
    [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=7,2048 rootfstype=ubifs rootwait=1ip=192.168.18.8:192.168.18.180:192.168.18.1:255.255.255.0::eth0:off
    [ 0.000000] PID hash table entries: 256 (order: -2, 1024 bytes)
    [ 0.000000] Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
    [ 0.000000] Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
    [ 0.000000] Memory: 64MB = 64MB total
    [ 0.000000] Memory: 59336k/59336k available, 6200k reserved, 0K highmem
    [ 0.000000] Virtual kernel memory layout:
    [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
    [ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
    [ 0.000000] vmalloc : 0xc4800000 - 0xff000000 ( 936 MB)
    [ 0.000000] lowmem : 0xc0000000 - 0xc4000000 ( 64 MB)
    [ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
    [ 0.000000] .text : 0xc0008000 - 0xc04be000 (4824 kB)
    [ 0.000000] .init : 0xc04be000 - 0xc04f3000 ( 212 kB)
    [ 0.000000] .data : 0xc04f4000 - 0xc054bd28 ( 352 kB)
    [ 0.000000] .bss : 0xc054bd4c - 0xc0576088 ( 169 kB)
    [ 0.000000] NR_IRQS:396
    [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [ 0.000000] Total of 128 interrupts on 1 active controller
    [ 0.000000] OMAP clockevent source: GPTIMER2 at 24000000 Hz
    [ 0.000000] OMAP clocksource: GPTIMER1 at 32768 Hz
    [ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
    [ 0.000000] Console: colour dummy device 80x30
    [ 0.000152] Calibrating delay loop... 548.86 BogoMIPS (lpj=2744320)
    [ 0.048706] pid_max: default: 32768 minimum: 301
    [ 0.048858] Security Framework initialized
    [ 0.048950] Mount-cache hash table entries: 512
    [ 0.049377] CPU: Testing write buffer coherency: ok
    [ 0.070800] omap_hwmod: gfx: failed to hardreset
    [ 0.087493] omap_hwmod: pruss: failed to hardreset
    [ 0.088775] print_constraints: dummy:
    [ 0.089202] NET: Registered protocol family 16
    [ 0.091705] OMAP GPIO hardware version 0.1
    [ 0.094482] omap_mux_init: Add partition: #1: core, flags: 0
    [ 0.097167] ehrpwm.0 regist succeed
    [ 0.097381] linux backlight regist succeed
    [ 0.147979] da8xx_lcdc_lidd.0: alias fck already exists
    [ 0.148254] BVS-pro LCD init succeed!!!
    [ 0.148315]
    [ 0.148315] adding i2c bus now
    [ 0.148315]
    [ 0.148376] omap_i2c.1: alias fck already exists
    [ 0.148681]
    [ 0.148681] adding i2c bus now
    [ 0.148681]
    [ 0.148712] omap_i2c.2: alias fck already exists
    [ 0.149414] CC2564MODN init done.
    [ 0.150665]
    [ 0.150665] start to init omap-gpmc
    [ 0.150665]
    [ 0.151428] _omap_mux_get_by_name: Could not find signal ain0.ain0
    [ 0.151458] _omap_mux_get_by_name: Could not find signal vrefp.vrefp
    [ 0.151489] _omap_mux_get_by_name: Could not find signal vrefn.vrefn
    [ 0.153198] edma.0: alias fck already exists
    [ 0.153228] edma.0: alias fck already exists
    [ 0.153259] edma.0: alias fck already exists
    [ 0.178314] bio: create slab <bio-0> at 0
    [ 0.180664] usbcore: registered new interface driver usbfs
    [ 0.181030] usbcore: registered new interface driver hub
    [ 0.181243] usbcore: registered new device driver usb
    [ 0.181427] musb-ti81xx musb-ti81xx: musb0, board_mode=0x12, plat_mode=0x2
    [ 0.181793] musb-ti81xx musb-ti81xx: musb1, board_mode=0x12, plat_mode=0x1
    [ 0.182983] omap_i2c omap_i2c.1: bus 1 rev2.4.0 at 100 kHz
    [ 0.198608] omap_i2c omap_i2c.2: bus 2 rev2.4.0 at 100 kHz
    [ 0.201446] Switching to clocksource gp timer
    [ 0.219360] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
    [ 0.219543] musb-hdrc musb-hdrc.0: dma type: pio
    [ 0.219879] MUSB0 controller's USBSS revision = 4ea20800
    [ 0.219909] musb0: Enabled SW babble control
    [ 0.220611] musb-hdrc musb-hdrc.0: USB Peripheral mode controller at c483c000 using PIO, IRQ 18
    [ 0.220733] musb-hdrc musb-hdrc.1: dma type: pio
    [ 0.221038] MUSB1 controller's USBSS revision = 4ea20800
    [ 0.221069] musb-hdrc musb-hdrc.1: host: value of mode reg=80 regval(80)
    [ 0.221069] musb1: Enabled SW babble control
    [ 0.221252] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
    [ 0.221374] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
    [ 0.221618] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    [ 0.221649] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [ 0.221649] usb usb1: Product: MUSB HDRC host driver
    [ 0.221679] usb usb1: Manufacturer: Linux 3.2.0-ga75e3d3 musb-hcd
    [ 0.221679] usb usb1: SerialNumber: musb-hdrc.1
    [ 0.222656] hub 1-0:1.0: USB hub found
    [ 0.222686] hub 1-0:1.0: 1 port detected
    [ 0.223419] musb-hdrc musb-hdrc.1: USB Host mode controller at c483e800 using PIO, IRQ 19
    [ 0.223907] NET: Registered protocol family 2
    [ 0.224121] IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
    [ 0.224487] TCP established hash table entries: 2048 (order: 2, 16384 bytes)
    [ 0.224548] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
    [ 0.224578] TCP: Hash tables configured (established 2048 bind 2048)
    [ 0.224609] TCP reno registered
    [ 0.224609] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.224639] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [ 0.224884] NET: Registered protocol family 1
    [ 0.225219] RPC: Registered named UNIX socket transport module.
    [ 0.225219] RPC: Registered udp transport module.
    [ 0.225219] RPC: Registered tcp transport module.
    [ 0.225250] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [ 0.225738] omap-gpmc omap-gpmc: GPMC revision 6.0
    [ 0.225738] Registering NAND on CS0
    [ 0.230712] VFS: Disk quotas dquot_6.5.2
    [ 0.230804] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    [ 0.231384] msgmni has been set to 115
    [ 0.235168] alg: No test for stdrng (krng)
    [ 0.235900] io scheduler noop registered
    [ 0.235931] io scheduler deadline registered
    [ 0.235992] io scheduler cfq registered (default)
    [ 0.236328] pwm register name is ehrpwm.0:0
    [ 0.236724] PWMSS: ehrpwm channel [0] init done!
    [ 0.236755] pwm register name is ehrpwm.0:1
    [ 0.237030] PWMSS: ehrpwm channel [1] init done!
    [ 0.237365] pwm_request: pwm name is ehrpwm.0:1
    [ 0.237396]
    [ 0.237396] ehrpwm: The clk freq is 100000000
    [ 0.237457] pwm-backlightpwm-backlight pwm-backlight: got pwm for backlight
    [ 0.238128] da8xx_lcdc_lidd da8xx_lcdc_lidd.0: lidd-fb:LCD_VERSION_2
    [ 0.238128] da8xx_lcdc_lidd da8xx_lcdc_lidd.0: GLCD: Found Topfoison_TF16002A-V0 panel
    [ 0.359527] da8xx_lcdc_lidd da8xx_lcdc_lidd.0: GLCD: FB kmalloc succeed!
    [ 0.359527] vram_size=0x1e000,vram_virt=0xffde0000,vram_phys=0x83f00000
    [ 0.360076] da8xx_lcdc_lidd da8xx_lcdc_lidd.0: GLCD: irq get succeed
    [ 0.363189] da8xx_lcdc_lidd da8xx_lcdc_lidd.0: GLCD: FB register succeed!
    [ 0.364044] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
    [ 1.074035] console [ttyO0] enabled
    [ 1.078674] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
    [ 1.086608] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
    [ 1.096923] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
    [ 1.104827] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
    [ 1.115112] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
    [ 1.123565] omap4_rng omap4_rng: OMAP4 Random Number Generator ver. 2.00
    [ 1.134185] loop: module loaded
    [ 1.137786] (stk) :sysfs entries created
    [ 1.141937] (stk) : debugfs entries created
    [ 1.150878] mtdoops: mtd device (mtddev=name/number) must be supplied
    [ 1.158294] omap2-nand driver initializing
    [ 1.165405] ONFI flash detected
    [ 1.168975] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xbc (Micron NAND 512MiB 1,8V 16-bit)
    [ 1.178314] Creating 8 MTD partitions on "omap2-nand.0":
    [ 1.184600] 0x000000000000-0x000000020000 : "SPL"
    [ 1.191192] 0x000000020000-0x000000040000 : "SPL.backup1"
    [ 1.198364] 0x000000040000-0x000000060000 : "SPL.backup2"
    [ 1.207794] 0x000000060000-0x000000080000 : "SPL.backup3"
    [ 1.214904] 0x000000080000-0x000000260000 : "U-Boot"
    [ 1.223937] 0x000000260000-0x000000280000 : "U-Boot Env"
    [ 1.230957] 0x000000280000-0x000000780000 : "Kernel"
    [ 1.240295] 0x000000780000-0x000020000000 : "File System"
    [ 1.461517] UBI: attaching mtd7 to ubi0
    [ 1.465606] UBI: physical eraseblock size: 131072 bytes (128 KiB)
    [ 1.472198] UBI: logical eraseblock size: 126976 bytes
    [ 1.477966] UBI: smallest flash I/O unit: 2048
    [ 1.482940] UBI: VID header offset: 2048 (aligned 2048)
    [ 1.489227] UBI: data offset: 4096
    [ 1.612274] usb 1-1: new full-speed USB device number 2 using musb-hdrc
    [ 1.784179] usb 1-1: New USB device found, idVendor=26f1, idProduct=8801
    [ 1.791198] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
    [ 1.798828] usb 1-1: Product: HIDKeyBoard
    [ 1.803070] usb 1-1: Manufacturer: TMS
    [ 1.806976] usb 1-1: SerialNumber: 1234567890abcd
    [ 4.207824] UBI: max. sequence number: 1657
    [ 4.228149] UBI: attached mtd7 to ubi0
    [ 4.232177] UBI: MTD device name: "File System"
    [ 4.238006] UBI: MTD device size: 504 MiB
    [ 4.243286] UBI: number of good PEBs: 4036
    [ 4.248199] UBI: number of bad PEBs: 0
    [ 4.252868] UBI: number of corrupted PEBs: 0
    [ 4.257568] UBI: max. allowed volumes: 128
    [ 4.262420] UBI: wear-leveling threshold: 4096
    [ 4.267333] UBI: number of internal volumes: 1
    [ 4.272003] UBI: number of user volumes: 1
    [ 4.276702] UBI: available PEBs: 0
    [ 4.281372] UBI: total number of reserved PEBs: 4036
    [ 4.286560] UBI: number of PEBs reserved for bad PEB handling: 40
    [ 4.292968] UBI: max/mean erase counter: 2/1
    [ 4.297485] UBI: image sequence number: 1593206285
    [ 4.302734] UBI: background thread "ubi_bgt0d" started, PID 454
    [ 4.352142] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
    [ 4.358612] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
    [ 4.368164] davinci_mdio.0: probed
    [ 4.371734] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver SMSC LAN8710/LAN8720
    [ 4.380798] mousedev: PS/2 mouse device common for all mice
    [ 4.389312] ==ft5x0x_ts_init==
    [ 4.392608] ==ft5x0x_ts_probe=
    [ 4.395812] we are using adapter: OMAP I2C adapter
    [ 4.400817] we get i2c0 work now
    [ 4.404266] ==kzalloc=
    [ 4.407714] input: ft5x06_ts as /devices/virtual/input/input0
    [ 4.472717] [FST] FT55x0x Firmware version = 0x0
    [ 4.478118] [FST] FT55x0x touch threshold = 25x
    [ 4.483978] [FST] FT55x0x touch threshold = 5x
    [ 4.488677] ==probe over =
    [ 4.491790] ret=0
    [ 4.495330] rtc-ds1307 2-0068: SET TIME!
    [ 4.500610] we will in rtc_device_register
    [ 4.507934] rtc-ds1307 2-0068: rtc core: registered ds1339 as rtc0
    [ 4.515106] omap_rtc am33xx-rtc: rtc core: registered am33xx-rtc as rtc1
    [ 4.524871] i2c /dev entries driver
    [ 4.529235] Linux media interface: v0.10
    [ 4.533599] Linux video capture interface: v2.00
    [ 4.541198] usbcore: registered new interface driver uvcvideo
    [ 4.547241] USB Video Class driver (1.1.1)
    [ 4.552368] OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [ 4.561340] _regulator_get: deviceless supply vdd_mpu not found, using dummy regulator
    [ 4.570159] cpuidle: using governor ladder
    [ 4.577087] cpuidle: using governor menu
    [ 4.581756] omap4_aes_mod_init: loading AM33X AES driver
    [ 4.587493] omap4-aes omap4-aes: AM33X AES hw accel rev: 3.02
    [ 4.596527] omap4_aes_probe: probe() done
    [ 4.600982] omap4_sham_mod_init: loading AM33X SHA/MD5 driver
    [ 4.607177] omap4-sham omap4-sham: AM33X SHA/MD5 hw accel rev: 4.03
    [ 4.622283] omap4_sham_probe: probe() done
    [ 4.627838] tiadc tiadc: attached adc driver
    [ 4.634918] oprofile: hardware counters not available
    [ 4.640228] oprofile: using timer interrupt.
    [ 4.644744] nf_conntrack version 0.5.0 (927 buckets, 3708 max)
    [ 4.653839] ip_tables: (C) 2000-2006 Netfilter Core Team
    [ 4.659545] TCP cubic registered
    [ 4.662963] NET: Registered protocol family 17
    [ 4.670715] Registering the dns_resolver key type
    [ 4.675750] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [ 4.684020] ThumbEE CPU extension supported.
    [ 4.688598] mux: Failed to setup hwmod io irq -22
    [ 4.694305] Power Management for AM33XX family
    [ 4.699157] Trying to load am335x-pm-firmware.bin (60 secs timeout)
    [ 4.708343] Copied the M3 firmware to UMEM
    [ 4.712738] Cortex M3 Firmware Version = 0x181
    [ 4.717926] sr_init: platform driver register failed
    [ 4.725708] clock: disabling unused clocks to save power
    [ 4.747955] Detected MACID=c4:ed:ba:8b:93:d8
    [ 4.753692] cpsw: Detected MACID = c4:ed:ba:8b:93:da
    [ 4.763031] input: gpio-keys as /devices/platform/gpio-keys/input/input1
    [ 4.771972] rtc-ds1307 2-0068: setting system clock to 2000-01-01 00:00:10 UTC (946684810)
    [ 4.823883] UBIFS: recovery needed
    [ 4.939727] UBIFS: recovery completed
    [ 4.944458] UBIFS: mounted UBI device 0, volume 0, name "rootfs"
    [ 4.950775] UBIFS: file system size: 97136640 bytes (94860 KiB, 92 MiB, 765 LEBs)
    [ 4.958862] UBIFS: journal size: 9023488 bytes (8812 KiB, 8 MiB, 72 LEBs)
    [ 4.966552] UBIFS: media format: w4/r0 (latest is w4/r0)
    [ 4.972656] UBIFS: default compressor: lzo
    [ 4.976959] UBIFS: reserved for root: 0 bytes (0 KiB)
    [ 4.985290] VFS: Mounted root (ubifs filesystem) on device 0:13.
    [ 4.992034] Freeing init memory: 212K
    INIT: version 2.88 booting
    Starting udev
    [ 7.414184] Disabling lock debugging due to kernel taint
    [ 7.423370]
    [ 7.423370] ProbeFPGA_char_init()
    [ 7.432464] EDMA channel 52 request successful!
    [ 7.437530] EDMA init mission accomplished!
    [ 7.442047] Power_OFF request failed!
    [ 7.445892] In_Charging request failed!
    [ 7.449920] LEDs init done!
    [ 7.452850] FPGA_DONE input as 0
    [ 7.456268] FPGA GPIO init done
    [ 7.459564] ProbeFPGA driver register & init completed!
    [ 7.459564]
    Configuring network interfaces... [ 8.242767] net eth0: CPSW phy found : id is : 0x7c0f1
    done.
    Tue Nov 19 22:47:00 UTC 2019
    INIT: Entering runlevel: 5
    Starting system message bus: Unknown username "pulse" in message bus configuration file
    dbus.
    Starting Dropbear SSH server: dropbear.
    Starting network benchmark server: netserver.
    This is a Mediate bladder scanner BVS-pro.
    Starting BVS-pro app...
    Stopping Bootlog daemon: bootlogd.

    _____ _____ _ _
    | _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
    | | _| .'| . | . | | __| _| . | | | -_| _| _|
    |__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
    |___| |___|

    Arago Project http://arago-project.org am335x-evm ttyO0

    Arago 2013.05 am335x-evm ttyO0

    am335x-evm login: "UTF-8"
    QFont( "DejaVu Sans,12,-1,5,50,0,0,0,0,0" )
    QFont( "WenQuanYi Micro Hei,12,-1,5,50,0,0,0,0,0" )
    nation is : "cn" load is true
    we're running in "/"
    start BVS-pro probe init
    [ 10.796539] FPGA open now.
    [ 10.813873]
    [ 10.813903] ehrpwm: The clk freq is 100000000
    [ 10.849182] write address is 0x0.
    [ 10.852691] write content is 32.
    [ 10.856140] FPGA write accomplished.
    [ 10.867584] write address is 0x2.
    [ 10.871063] write content is 4.
    [ 10.874359] FPGA write accomplished.
    [ 10.883300] write address is 0x4.
    [ 10.886779] write content is 45000.
    [ 10.890441] FPGA write accomplished.
    [ 10.899291] write address is 0x8.
    [ 10.902770] write content is 40000.
    [ 10.906433] FPGA write accomplished.
    [ 10.915252] write address is 0xc.
    [ 10.918731] write content is 40.
    [ 10.922119] FPGA write accomplished.
    [ 10.930938] write address is 0xe.
    [ 10.934417] write content is 15365.
    [ 10.938079] FPGA write accomplished.
    [ 10.950103] write address is 0x14.
    [ 10.953735] write content is 389.
    [ 10.957183] FPGA write accomplished.
    [ 10.966278] write address is 0x16.
    [ 10.969848] write content is 8.
    [ 10.973114] FPGA write accomplished.
    [ 10.982025] write address is 0x1a.
    [ 10.985595] write content is 15.
    [ 10.988983] FPGA write accomplished.
    [ 10.997833] write address is 0x1c.
    [ 11.001403] write content is 2600.
    [ 11.004974] FPGA write accomplished.
    [ 11.013824] write address is 0x86.
    [ 11.017395] write content is 29491.
    [ 11.021057] FPGA write accomplished.
    [ 11.029937] write address is 0x88.
    [ 11.033508] write content is 1.
    [ 11.036804] FPGA write accomplished.
    [ 11.045593] write address is 0x8a.
    [ 11.049163] write content is 64766.
    [ 11.052795] FPGA write accomplished.
    [ 11.064361] write address is 0x8c.
    [ 11.067932] write content is 1736.
    [ 11.071472] FPGA write accomplished.
    [ 11.080474] write address is 0x8e.
    [ 11.084045] write content is 62856.
    [ 11.087707] FPGA write accomplished.
    [ 11.096557] write address is 0x90.
    [ 11.100128] write content is 19459.
    [ 11.103790] FPGA write accomplished.
    [ 11.112640] write address is 0x92.
    [ 11.116210] write content is 62856.
    [ 11.119842] FPGA write accomplished.
    [ 11.128723] write address is 0x94.
    [ 11.132263] write content is 1736.
    [ 11.135833] FPGA write accomplished.
    [ 11.144714] write address is 0x96.
    [ 11.148254] write content is 64766.
    [ 11.151916] FPGA write accomplished.
    [ 11.160766] write address is 0x20.
    [ 11.164337] write content is 4.
    [ 11.167633] FPGA write accomplished.
    call c func end, our pid is 959
    open db succeed.

    db version code: 2
    scanTime Column index: 5
    open db in BVSpro(), records : 0
    brightness 50
    brightness 50
    sleeptime 8 ; offtime 8
    [ 11.436859] write address is 0x18.
    [ 11.440643] write content is 1.
    [ 11.444030] FPGA write accomplished.
    [ 11.468811] write address is 0x18.
    [ 11.472381] write content is 0.
    [ 11.476898] FPGA write accomplished.
    [ 11.485900] write TGC FIFO accomplished!
    [ 11.490020] FPGA write accomplished.
    [ 11.499053] write address is 0x22.
    [ 11.502624] write content is 1026.
    [ 11.506195] FPGA write accomplished.
    TGC 100 ; motorphase 1026
    in screensaver::restore now
    connect succeed
  • 看到您已经回复,请跟进,谢谢。
  • 那个帖子进不去了,请问是怎么回事呢?

  • 英文论坛可能是在升级,周一应该是可以正常回复的。