This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678固化启动以及仿真调试的问题



1.C6678外挂了S29GL01GP ,使用裸机工程可以将bin文件烧写进去,将程序固化

2.用户工程使用了sys/bios=6.33.4.39,CCS版本为5.5,MCSDK=2.0.9.21,PDK=1.0.0.21,NDK=2.21.0.32

所有核运行在一个用户工程里,调试用户工程时遇到以下问题:

    1)局部变量时高维的,系统堆栈不够用,希望整个工程放在DDR3中运行,怎么把FLASH中的程序搬移到DDR3中运行?

    2)使用仿真器调试时,需要使用gel文件初始化DDR3?如果程序需要固化,时钟、DDR3、UART、SRIO、EMIF等初始化程序怎么放在二级引导程序里?

    3)需要多DDR3进行分区管理吗?每个核运行在DDR3中不同区域里。