If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是错误提示
C55xx: GEL Output: Gel StartUp Complete.
C55xx: GEL Output: C5509 Memory Map Initialization Complete.
C55xx: Trouble Reading Memory Block at 0x2024 on Page 1 of Length 0x1: (Error -1144 @ 0x2024) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2424 on Page 1 of Length 0x1: (Error -1144 @ 0x2424) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2025 on Page 1 of Length 0x1: (Error -1144 @ 0x2024) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2824 on Page 1 of Length 0x1: (Error -1144 @ 0x2824) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2425 on Page 1 of Length 0x1: (Error -1144 @ 0x2424) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2002 on Page 1 of Length 0x2: (Error -1144 @ 0x2002) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2026 on Page 1 of Length 0x1: (Error -1144 @ 0x2026) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2000 on Page 1 of Length 0x1: (Error -1144 @ 0x2000) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2825 on Page 1 of Length 0x1: (Error -1144 @ 0x2824) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2426 on Page 1 of Length 0x1: (Error -1144 @ 0x2426) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2004 on Page 1 of Length 0x2: (Error -1144 @ 0x2004) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2027 on Page 1 of Length 0x1: (Error -1144 @ 0x2026) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2d34 on Page 1 of Length 0x2: (Error -1144 @ 0x2D34) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2826 on Page 1 of Length 0x1: (Error -1144 @ 0x2826) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2dc9 on Page 1 of Length 0x1: (Error -1144 @ 0x2DC8) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2427 on Page 1 of Length 0x1: (Error -1144 @ 0x2426) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x492 on Page 1 of Length 0x1: (Error -1144 @ 0x492) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2006 on Page 1 of Length 0x2: (Error -1144 @ 0x2006) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2028 on Page 1 of Length 0x1: (Error -1144 @ 0x2028) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2827 on Page 1 of Length 0x1: (Error -1144 @ 0x2826) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2428 on Page 1 of Length 0x1: (Error -1144 @ 0x2428) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x493 on Page 1 of Length 0x1: (Error -1144 @ 0x492) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2008 on Page 1 of Length 0x2: (Error -1144 @ 0x2008) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x2828 on Page 1 of Length 0x1: (Error -1144 @ 0x2828) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x494 on Page 1 of Length 0x1: (Error -1144 @ 0x494) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x200a on Page 1 of Length 0x2: (Error -1144 @ 0x200A) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x495 on Page 1 of Length 0x1: (Error -1144 @ 0x494) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Trouble Reading Memory Block at 0x496 on Page 1 of Length 0x1: (Error -1144 @ 0x496) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
C55xx: Error: (Error -1144 @ 0x400) Device core is hung. The debugger attempted to recover debug control, but was unsuccessful. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
/*H***************************************************************************
* $Revision: /main/c55x_rel/c55xx_ccs240/2 $
* $Date: July 28, 2004 11:27:36 $
*
* TI Proprietary Information - Internal Data
* Copyright (c) 2004, Texas Instruments Incorporated
* All rights reserved
*****************************************************************************/
/* The Startup() function is executed when the GEL file is loaded. */
/* Initialize the EMIF control registers to access */
/* SBSRAM(CE0), FLASH(CE1), CPLD control & status regs(CE3) */
hotmenu C5509_USB_Enable()
{
GEL_MemoryFill(0x7000,2,1,0x0004);
GEL_TextOut("C5509 USB Module enabled.\n");
}
menuitem "C5509 EBSR Config";
hotmenu Data_EMIF_En()
{
GEL_MemoryFill(0x6C00,2,1,0x0200);
GEL_TextOut("C5509 Ext. Bus set to Data EMIF.\n");
}
hotmenu Full_EMIF_En()
{
GEL_MemoryFill(0x6C00,2,1,0x0201);
GEL_TextOut("C5509 Ext. Bus set to Full EMIF.\n");
}
hotmenu NonMuxed_EHPI_En()
{
GEL_MemoryFill(0x6C00,2,1,0x0202);
GEL_TextOut("C5509 Ext. Bus set to Non Muxed EHPI.\n");
}
hotmenu MuxEHPI_En()
{
GEL_MemoryFill(0x6C00,2,1,0x0203);
GEL_TextOut("C5509 Ext. Bus set to Muxed EHPI.\n");
}
menuitem "C5509 EMIF CE0 Config";
hotmenu CE0_Async16_En()
{
GEL_MemoryFill(0x0803,2,1,0x1FFF);
GEL_TextOut("C5509 CE0 set to 16-bit Async mode.\n");
}
menuitem "C5509 EMIF CE1 Config";
hotmenu CE1_Async16_En()
{
GEL_MemoryFill(0x0806,2,1,0x1FFF);
GEL_TextOut("C5509 CE1 set to 16-bit Async mode.\n");
}
menuitem "C5509 EMIF CE2 Config";
hotmenu CE2_Async16_En()
{
GEL_MemoryFill(0x0809,2,1,0x1FFF);
GEL_TextOut("C5509 CE2 set to 16-bit Async mode.\n");
}
menuitem "C5509 EMIF CE3 Config";
hotmenu CE3_Async16_En()
{
GEL_MemoryFill(0x080C,2,1,0x1FFF);
GEL_TextOut("C5509 CE3 set to 16-bit Async mode.\n");
}
/* Initialize Test Mode Control Registers(TMCR) */
/* This register selects modes for factory test */
/* and may be corrupted when device is powered */
/* up with the emulator attached. This */
/* function restores the the registers to their */
/* default values. There is not impact to */
/* system functionality from these writes. */
TMCR_Reset()
{
#define TMCR_MGS3 0x07FE
#define TMCR_MM 0x07FF