This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SEED-XDS510PLUS仿真器连接问题

Other Parts Discussed in Thread: TMS320C5535

我使用的是CCS5.2版本,用的TMS320C5535,SEED-XDS510PLUS仿真器驱动安装了,但是连接上SEED-XDS510PLUS仿真器时,进行Test connection时,出现了以下错误:

The controller has a version number of '1' (0x00000001).
The controller has an insertion length of '16' (0x00000010).
This utility will attempt to reset the controller.

A error occurred while attempting to reset the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-342' (0xfffffeaa).
The title is 'SC_ERR_HUNG_COMMAND'.

The explanation is:
Failure due to the controller command-finish taking too long.

[End]