This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSS VNF与ISS VNF的区别?

我现在用的是DM8127,跑的时IPNC3.5。有以下几个问题

1、DSS VNF与ISS VNF的区别?

2、VNF包括NSF和TNF吗?VNF就是所谓的3D滤波吗?

3、 VNF对图像大小是否有限制?

4、VNF需要运行在fullfeature模式还是lowpower模式

  • 1. 一个是硬3D去噪,一个是软件。DSS的性能较高,在噪声很大的情况下抑制没有ISS的好。

    2. 两个都是3D去噪

    3.请问你需要处理多大分辨率?

    4. ISS VNF两种都可以,但TI的demo是放在full feature里面的。

  • hi,Chris Meng

    万分感谢!

    我现在用ISS VNF,采集的图像大小是2448*2432

    1、降噪后的图像为什么变成了2416*2400

    2、终端出现如下错误信息:

    [m3vpss ] Error :: src/msp_vnf.c : MSP_VNF_CheckParams : 4861 :: Exiting because : pCreateParam->ulInputStride % 32 != 0

    但此时3D降噪也起作用了,这个错误信息很重要码?