我们使用的SDK配置文件是processor-sdk-06.03.00.106-config.txt。
按照以下帖中所说的步骤。

在tisdk的conf/local.conf文件末尾添加PACKAGECONFIG_append = " sql-sqlite"。再执行MACHINE=am57xx-evm bitbake qtbase。会报错,无法正常编译。报的错是:
ERROR: initscripts-1.0-r155 do_configure: Function failed: do_configure (log file is located at /home/zhang/tisdk/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/initscripts/1.0-r155/temp/log.do_configure.51765)
完整编译信息如下:
/tisdk/build$ MACHINE=am335x-evm bitbake qtbase
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
Loading cache: 100% |###########################################| Time: 0:00:03
Loaded 4658 entries from dependency cache.
WARNING: No recipes available for:
/home/zhang/tisdk/tisdk/sources/meta-arago/meta-arago-distro/recipes-browser/chromium/chromium-wayland_%.bbappend
/home/zhang/tisdk/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/move-base_1.12.14.bbappend
/home/zhang/tisdk/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/rotate-recovery_1.12.14.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.40.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-18.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am335x-evm"
DISTRO = "arago"
DISTRO_VERSION = "2019.11"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:56d9d47f18eeec31a1086ca29e54b5956c46de84"
meta-aws = "HEAD:6432f1b38b9dcbbb55020167f5b1cfe55e858c6d"
meta-ros = "HEAD:72068b17e4192b51e09c8dc633805a35edac8701"
meta-arago-distro
meta-arago-extras = "HEAD:70436496d2617b281c51390faa3d421814055cd6"
meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"
meta-qt5 = "HEAD:e6e464c9ed9266ce46452f953c1bdcb0e7b2d95f"
meta-virtualization = "HEAD:7685c7d415e0002c448007960837ae8898cd57a5"
meta-networking
meta-python
meta-oe
meta-gnome
meta-multimedia
meta-filesystems = "HEAD:446bd615fd7cb9bc7a159fe5c2019ed08d1a7a93"
meta-ti = "HEAD:b27317ab4f9be931a66344ca502c7e3f4ec780e5"
meta-linaro-toolchain
meta-optee = "HEAD:615ea7561b844a3867cee4299d83d605c10b02ab"
meta = "HEAD:e68991ceb5933f7d03b96697e8a0ba0829feb320"
Initialising tasks: 100% |######################################| Time: 0:00:01
Sstate summary: Wanted 350 Found 0 Missed 350 Current 7 (0% match, 1% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: initscripts-1.0-r155 do_configure: Function failed: do_configure (log file is located at /home/zhang/tisdk/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/initscripts/1.0-r155/temp/log.do_configure.51765)
ERROR: Logfile of failure stored in: /home/zhang/tisdk/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/initscripts/1.0-r155/temp/log.do_configure.51765
Log data follows:
| DEBUG: Executing shell function do_configure
| sed: can't read /home/zhang/tisdk/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/initscripts/1.0-r155/halt: No such file or directory
| WARNING: /home/zhang/tisdk/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/initscripts/1.0-r155/temp/run.do_configure.51765:1 exit 2 from 'sed -i -e "s:SED_HALTARGS:-d -f:g" /home/zhang/tisdk/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/initscripts/1.0-r155/halt'
| ERROR: Function failed: do_configure (log file is located at /home/zhang/tisdk/tisdk/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/initscripts/1.0-r155/temp/log.do_configure.51765)
ERROR: Task (/home/zhang/tisdk/tisdk/sources/oe-core/meta/recipes-core/initscripts/initscripts_1.0.bb:do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 358 tasks of which 355 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/zhang/tisdk/tisdk/sources/oe-core/meta/recipes-core/initscripts/initscripts_1.0.bb:do_configure
Summary: There were 3 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.