This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am437x网卡启动



am437x配置网口启动,确认网口IO是正确的,启动sysboot引脚也是正确配置的,按照正常流程应该是BOOTROM程序通过BOOTIP协议从PC端的hdcp服务器中获取动态ip地址的,但上电启动没任何反应,调试串口没任何输出,PC上用wireshark工具检测网卡没有发现任何DHCP请求包,用示波器测量网口的相关IO口,rmii1_tx[1:0]没有任何信号,rmii1_txen也是没信号,是否和这有关系?

PC上的CCS UNflash是正常运行的,dhcp服务器也是正常工作的,这个都是有验证过的。

PS:通过其他方式启动板卡,板卡上的网络也是正常可用的,证明板子上网络硬件是正常的。

PS;配置官方AM437x_GP_EVM开发板从网络启动,是能正常获取ip地址的,对比官方开发板原理图和我们自己的原理图,差别应该就是官方使用的是RGMII,而我们使用的是RMII方式。